Skip to main content

Renesas Blog

Renesas Functional Safety Support for Automotive (3) – Applying the ISO 26262 Standard to SEooC Software

Renesas Functional Safety Support for Automotive (3) – Applying the ISO 26262 Standard to SEooC Software

This blog presents ISO 26262 guidance on developing Safety Element out of Context (SEooC) software, the challenges encountered during SEooC software development, and Renesas SEooC software solutions.

Completing Setup in Just 30 Minutes! Introducing the New Development Environment for Connected Cars by Renesas

Completing Setup in Just 30 Minutes! Introducing the New Development Environment for Connected Cars by Renesas

Using the Connected Car Platform - Starter Kit (CCPF-SK), R-Car users can set up the development environment for connected cars easily and quickly and focus on the development of added value software.

Embedded Artificial Intelligence Inference with Renesas RZ/G2

Embedded Artificial Intelligence Inference with Renesas RZ/G2

Introducing the RZ/G Free and Open Source Software (FOSS) AI Board Support Package (BSP) that includes popular Open Source AI frameworks and sample benchmarking applications for each framework.

Run a motor with encoder interface by using RA6T1 motor control RSSK

Run a Motor with Encoder Interface Using the RA6T1 Motor Control RSSK

Learn how to extract the parameters of a user’s own motor using the Renesas Motor Workbench’s tuner function with the RA6T1 MCU and how to fill the parameters into the sample program.

Improve UX/UI with RX140 MCU Equipped with A New Generation of Capacitive Touch Sensor

Improve UX/UI with RX140 MCU Equipped with A New Generation of Capacitive Touch Sensor

The RX140 in the RX100 MCUs contribute to improved device performance and lower power consumption and feature the latest touch-key IP to further enhance the design and usability of customer products.

What is data acquisition (DAQ) and distributed processing/edge computing in the IoT era with RX23E-A?

What is Data Acquisition (DAQ) and Distributed Processing/Edge Computing in the IoT Era with RX23E-A?

When combining RX23E-A, a microcontroller with high precision AFE, with RX72M, a microcontroller with enhanced function for industrial network, you can realize data acquisition (DAQ) for the IoT era.

Dataline performance of two new actors in the networking arena

The Art of Networking (Series 4): CAN XL and 10BASE-T1S – Dataline Performance of Two New Actors in the Networking Arena

This blog gives a brief overview of CAN XL and 10MBit/s Ethernet, and the differences between them.

Functional Safety over EtherCAT Blog

How Renesas Approaches Functional Safety over EtherCAT (FSoE)

This blog focuses on how Renesas’ Functional Safety over EtherCAT (FSoE) solution simplifies development and shortens development time.

Obtain the Latest Information at the “Virtual Renesas Automotive Days”!

Obtain the Latest Information at the “Virtual Renesas Automotive Days”!

“Virtual Renesas Automotive Days” is an opportunity for Renesas to update you on its strategy and broad lineup of automotive solutions.

RX72M Single-Chip Motor Control via EtherCAT Communications

RX72M Single-Chip Motor Control via EtherCAT Communications

To solve recent factory automation issues, Renesas proposes an RX72M Motor + EtherCAT single-chip solution, which realizes application processing, standard EtherCAT communication and motor control.