メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)

RZ/G3E MPU Tutorial: Low‑Power Mode and Fast Resume Feature

RZ/G3E MPU Tutorial: Low‑Power Mode and Fast Resume Feature
2025年12月21日

このビデオについて

We will show you the key features of Renesas’ RZ/G3E microprocessor, focusing on its low-power mode and fast resume capability through a hands-on demonstration. 

The RZ/G3E evaluation board is connected to a Windows PC, and a current measurement program is used to monitor power consumption across each power domain. After Linux boots, the system transitions to sleep mode, shutting down multiple power domains completely while keeping DDR in self-refresh mode to retain the Linux image. As a result, power consumption is significantly reduced, which can be clearly observed in the graphs.