概要
The Renesas Demonstration Kit (RDK) for RX62N is an evaluation and demonstration tool for Renesas RX62N microcontrollers. The goal is to provide the user with a powerful debug and demonstration platform targeted at common applications. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using the High-performance Embedded Workshop (HEW) IDE as well as programming the device using the on-board SEGGER J-Link JTAG debugger.
The Renesas Demonstration Kit for RX62N is also the hardware platform that is included in a special RX62N-specific edition of Micrium's book on the µC/OS-III Real Time Kernel. The book and board combo targets serious programmers and college students who need to understand and create programs based on the timesaving features of a real-time kernel. Part I of the text covers the internals of the new µC/OS-III real-time kernel. The emphasis is on the internals, features, API calls, and where and how to use an RTOS, all presented in a clear and useful way, and accompanied by a wealth of diagrams. Part II provides specific examples for using µC/OS-III on the new Renesas RX62N microcontroller.
特長
- Stereo audio driver connected to the PWM interface
- On-board microphone to demonstrate sampling, FFT/FPU capabilities
- Volume Control Potentiometer
- Micro SD card interface for audio and data files
- 3-Phase motor control algorithm representation with LEDs
- Motor control algorithm speed variation through volume control potentiometer
- 3-Axis Accelerometer (Digital)
- User pushbutton switches
- 10/100 Etherface connected to an internal EthernetMAC (1588 compatible)
- USB Interface connected to an internal USB controller (Host, Device and OTG)
- RS-232 Interface
- CAN Interface
- I*C, SPI with Debug through the Beagle connector from Total Phase
- On-board J-link Lite for high-quality source code debugging
- User circuit breadboard area
サンプル&ご購入
YRDKRX62N
廃止品| Pb (Lead) Free: | No |
| ECCN (US): | 3A991.a.2 |
| HTS (US): | 8471.50.0150 |
| RoHS Compliant: | No |
| China RoHS Compliant: | No |