Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The Renesas Demonstration Kit (RDK) for RX62N is an evaluation and demonstration tool for Renesas RX62N microcontrollers. The goal is to provide the user with a powerful debug and demonstration platform targeted at common applications. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using the High-performance Embedded Workshop (HEW) IDE as well as programming the device using the on-board SEGGER J-Link JTAG debugger.

The Renesas Demonstration Kit for RX62N is also the hardware platform that is included in a special RX62N-specific edition of Micrium's book on the µC/OS-III Real Time Kernel. The book and board combo targets serious programmers and college students who need to understand and create programs based on the timesaving features of a real-time kernel. Part I of the text covers the internals of the new µC/OS-III real-time kernel. The emphasis is on the internals, features, API calls, and where and how to use an RTOS, all presented in a clear and useful way, and accompanied by a wealth of diagrams. Part II provides specific examples for using µC/OS-III on the new Renesas RX62N microcontroller.

Features

  • Stereo audio driver connected to the PWM interface
  • On-board microphone to demonstrate sampling, FFT/FPU capabilities
  • Volume Control Potentiometer
  • Micro SD card interface for audio and data files
  • 3-Phase motor control algorithm representation with LEDs
  • Motor control algorithm speed variation through volume control potentiometer
  • 3-Axis Accelerometer (Digital)
  • User pushbutton switches
  • 10/100 Etherface connected to an internal EthernetMAC (1588 compatible)
  • USB Interface connected to an internal USB controller (Host, Device and OTG)
  • RS-232 Interface
  • CAN Interface
  • I*C, SPI with Debug through the Beagle connector from Total Phase
  • On-board J-link Lite for high-quality source code debugging
  • User circuit breadboard area

Applications

Type Title Date
Manual - Development Tools PDF 3.91 MB
Quick Start Guide PDF 91 KB
Quick Start Guide PDF 96 KB
Quick Start Guide PDF 108 KB
4 items

Software & Tools

Software Downloads

Type Title Date
Software & Tools - Other
Log in to Download ZIP 829.29 MB
1 item
Part NumberStatusStockSampleablePb (Lead) FreeECCN (US)HTS (US)RoHS CompliantChina RoHS Compliant
YRDKRX62NObsoleteOut of StockN/ANo3A991.a.28471.50.0150NoNo

Support Communities

  1. SPI on YRDKRX62N

    Hello, I want to perform SPI communication between YRDKRX62N and a slave. SPI0 can communicate with 4 slaves. However, according to the pin definitions in the library and the attached diagram on the Kit, these slave select pins have been specially configured for modules such as Wifi, LCD, Flash, and ...

    Nov 15, 2023
  2. Problem with LCD on yrdkrx62n

    LCD doesn't work if PORT2.DDR.BYTE = 0x1A and by doesn't work, I mean it will not display backlight, so you can't see anything on it. By changing value to 0x18, or to 0, LCD backlight works ok.

    Apr 23, 2012
  3. Errors in Schematics of YRDKRX62N rev.3

    I do not know, how much errors are in that doc, because I did not follow all components, linesand addresses. But I was searching something and found on page 7(total 9) the signal and component numbering of LED ARRAY and LED RESISTORS not logical, in other words, it is ...

    Jan 6, 2011
View All Results from Support Communities (50)