メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)
代替製品

概要

説明

The VersaClock® 3S-5P3502x programmer board is made to ease the programming of blank 5P35021 and 5P35023 devices. With the on-board USB interface, the Renesas Timing Commander™ graphical user interface (GUI) is used to communicate with the blank device in the socket for configuration and programming.

特長

  • Program VersaClock 3S – 5P3502x blank parts in the socket
  • Removable socket board
    • EVK5P35021PROG is a VersaClock 3S USB programmer board with a QFN20 socket board for the 5P35021 device
    • EVK5P35023PROG is a VersaClock 3S USB programmer board with a QFN24 socket board for the 5P35023 device
  • Programmer board is powered by USB port
  • Programmer board uses Renesas Timing CommanderTM GUI to program the blank parts
  • USB port is the communication channel between the GUI and the VersaClock 3S–5P3502x device in the socket

アプリケーション

ドキュメント

設計・開発

ソフトウェア/ツール

ソフトウェアダウンロード

製品選択

Part NumberStatusStockSampleable
EVK5P35021PROGActiveOut of StockN/A
EVK5P35023PROGActiveOut of StockN/A

ビデオ&トレーニング