メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)

ブログ

Easy to Start with Tutorial Videos! Cloud Connectivity Using Azure RTOS and RX65N Cloud Kit Blog

動画で簡単スタート! Azure RTOS×RX65N Cloud Kitクラウド接続

Azure IoT Hubに接続し、アップロードしたデータを可視化する方法を動画で学んでみませんか? はじめての方に最適な、20分程度のチュートリアル動画をご紹介します。

Single Board Computer Blog

Renesas' Next-Generation AI Solution – Single Board Computer with Cortex-A55 Core

A compact, single-board computer using next-generation Arm® Cortex®-A55 core with an optimized bill of material is ideally suited for Edge-AI applications.

Voice Command on an Embedded Device Using the Commercially Available RX72N Kit Blog

市販のキットですぐに試せる、組込向け音声コマンドの導入

RXファミリのフラッグシップであるRX72Nのキットを使って、音声コマンドによる機器操作を試す方法をご紹介します。市販の安価なキットだけですぐに試すことが出来ます。

What’s New in Bluetooth® 5.3 Low Energy

What’s New in Bluetooth® 5.3 Low Energy

This blog presents an overview of the latest Bluetooth Low Energy (LE) specification release 5.3 and the value those new features will bring to Renesas customers and their next-generation designs.

Faster Evaluation Process with Unified and Scalable SMARC EVK Platform (Evaluation Board Kit Platform) Blog

統合されたスケーラブルなSMARC EVK プラットフォーム(評価キットプラットフォーム)により、 評価プロセスを迅速化

統合されたスケーラブルなSMARC EVK プラットフォームにより、お客様はCPU組込みモジュールを交換することで、製品を迅速に評価し、製品ラインナップの拡大が容易になります。

Get IoT Ready with Building Blocks from the Renesas Ready Partner Network Blog

Get IoT Ready with Building Blocks from the Renesas Ready Partner Network

Providing coverage across all mainstream Renesas MCUs from 8 to 32 bits, the Renesas Ready Partner Network makes it simple to find and integrate solutions tailored to your requirements.

Contributes to reduction of ROM / RAM usage by 8-bit quantization Released e-AI Translator V2.1.0 for TensorFlow Lite

8bit量子化技術でROM/RAM使用量削減に貢献 TensorFlow Liteに対応したe-AI Translator V2.1.0をリリース

「組み込みシステムでAIを活用したいが、ROM/RAMサイズに制約があり困っている」こんなお悩みをよく伺います。 このような課題の解決に最適なe-AIトランスレータ V2.1.0を9月30日にリリースしました。 “TensorFlow Lite”によって8bit量子化されたAIの学習済みモデルに対応することで、ニューラルネットワークのROM/RAM使用量を削減できます。
Interview with RX Family User, HITACHI Solutions Technology

RXファミリ ユーザインタビュー 日立ソリューションズ・テクノロジー

実開発で見えてきたRXの隠れた特長!~システム性能や機能up、将来を見据えた開発が容易~

The Art of Networking (Series 5): CAN XL and 10BASE-T1S – Gateway Performance of Two New Actors in the Networking Arena

The Art of Networking (Series 5): CAN XL and 10BASE-T1S – Gateway Performance of Two New Actors in the Networking Arena

In this post, we will look at how the 10BASE-T1S and CAN XL protocols could be used in a system and what is necessary to connect CAN XL and 10BASE-T1S to an IVN backbone.