Feb 28, 2025
About This Video
Renesas introduces the DA14533, an automotive AEC-Q100 grade 2 qualified Bluetooth® Low Energy System-on-Chip (SoC). The DA14533 is the latest addition to the successful SmartBond™ TINY family of products, providing ultra-low power Bluetooth functionality in the smallest footprint and integrating a 2.4GHz transceiver and an Arm® Cortex®-M0+ MCU with 64kB of RAM and 12kB of one-time programmable (OTP) memory.