Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

This product provides OpenCV Accelerator Support Package for RZ/V2L.
Please read the Release Note included in this first when you use the package.

[Feature]
OpenCV Accelerator Software

[Note]
The following packages is required to use this product.

Release Information

Feb.26,2024: OpenCV Accelerator Support Package V1.10

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 4.91 MB
1 item
Type Title Date
Application Note PDF 248 KB
AI-generated Summary: The OpenCV Accelerator Sample Application demonstrates executing various OpenCV functions on the RZ/V2L platform, with and without the DRP enabled. It covers image processing tasks such as resizing, color space conversion, Gaussian blur, dilation, erosion, morphology, convolution, edge detection, adaptive thresholding, template matching, affine and perspective transformations, and image scaling. The sample runs these functions sequentially on FHD images, highlighting performance differences between CPU and DRP execution. The document also details the required operating environment, software setup, compilation steps, and memory mapping for efficient use of the OpenCV Accelerator.
Manual - Software PDF 454 KB
Release Note PDF 358 KB
3 items

Related Boards & Kits

Support Policy

Renesas provides support for the items below for RZ/V2L OpenCV Accelerator Support Package without additional payment.

 FormQ&A and issue analysis*1Maintained by Renesas
Renesas reference boardCustomer board
Customer developed/modified SW-NoNo*2No
Customer added OSS-NoNoNo
Renesas developed SWSource CodeYesYesYes
BinaryYesYes*3Yes

*Notes:

  1. Firstly, customers should investigate which part has a problem: Renesas’ deliverables or customer’s developed part.
  2. We provide support for the board-dependent changes such as channel numbers and pin configurations.
  3. We provide Q&A support only for the functions which are defined and described in the user's manual.