Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

This is a MATLAB®/Simulink® model of the peripheral functions installed on the actual device. It provides simulation blocks that reproduce hardware for motor/inverter control with high accuracy. By combining this blockset and user model, it is possible to examine and check the operation of an actual system on the model.

MATLAB®, Simulink® are trademarks or registered trademarks of The MathWorks, Inc.

Features

  • Provides Simulink models of the peripheral functions installed on the actual device.
    • Timer RDe (TRD)
    • 12-bit A/D Converter (AD)
    • Application Accelerator Unit (AAU)

Target Devices

Type Title Date
Guide PDF 1.41 MB 日本語
1 item

For inquiries about this item, please contact the distributors or dealers.

Contact by email: mbd-solution-support@lm.renesas.com