Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

IECUBE

PG-FP5

The power-supply adapter is used for the full-spec emulator IECUBE and the programmer PG-FP5.

Target Devices

RegionModel No.Shipment after modification of the Safety Standard
IEC 62368-1 *Important 2
JapanQB-COMMON-PW-JPno change
AmericaQB-COMMON-PW-EAno change
EuropeBundled with the IECUBE and PG-FG5
(not separated)
no change
ChinaQB-COMMON-PW-CNThe order acceptance has been closed.
Hong KongQB-COMMON-PW-HKThe order acceptance has been closed.
KoreaQB-COMMON-PW-KRThe order acceptance has been closed.
SingaporeQB-COMMON-PW-SGThe order acceptance has been closed.
TaiwanQB-COMMON-PW-TWThe order acceptance has been closed.

Important :

  1. The power supply adapter is shipped only for orders from the destination area. For model numbers in other regions than above, contact one of the Renesas Electronics distributors or sales representatives in your area.
  2. In response to modification of the Safety Standard IEC62368-1, we discontinued our production of these power adapters "QB-COMMON-PW-xx" for the IECUBE and PG-FP5 (Discontinued product) which are intended to use in Asia excluding Japan.
    We also stop shipment of the IECUBE to Asia because there are no replacements for these power adapters.
    We will continue shipment to Japan, U.S., and Europe as we have done till now.