Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

This tool is an in-house tool that allows us to provide PCI Express IP with the requested configuration.

Users can visually configure the root complex/endpoint/retimer settings, rate settings (Gen1/Gen2/Gen3/Gen4/Gen5), AXI settings, and the next settings. Once the settings are complete, we can provide the RTL by obtaining the definition file, configuration sheet, terminal specification, performance sheet, and register specification.

Target Devices

Resources

Supported IP

FunctionIP NameStatus
PCI Express Link ControllerPCI Express 1.0 Link ControllerAvailable
PCI Express 2.0 Link ControllerAvailable
PCI Express 3.0 Link ControllerAvailable
PCI Express 4.0 Link ControllerAvailable
PCI Express 5.0 Link ControllerAvailable

Contact Us

For inquiries about PCI Express Configuration Tool, please contact us.

Contact Us


Support Communities

  1. ADAS Starter Kit H2

    Hello all, We have been working in the development of R-Car H2 and we have successfully compiled the OpenCV program using gcc compiler. Can anyone guide us the steps to compile (cross compile) OpenCV program for R-Car H2? Thanks and Regards, Vikram

    Jul 14, 2017