Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Embedded Target for RH850 Virtual Platform is a development environment that generates peripheral code for target devices from Simulink® models and enables cooperative verification as Virtual Hardware In the Loop Simulation (vHILS) in a virtual environment with Simulink.
Embedded Target for RH850 Virtual Platform and Board is a development environment that generates peripheral code for target devices from Simulink® models, enabling both vHILS and device verification using evaluation boards.

  • Peripheral code is generated from Simulink models, along with the algorithm code, making it easy to check the operation and evaluate the performance of the application including peripheral functions for device selection and prototyping, even if you are not familiar with device specifications.
  • When using a virtual environment, early verification is possible even before the device WS is completed, and verification can be performed without actual device.
  • When using an evaluation board, verification can be performed on the actual device after the device WS is completed.
Image
Overflow of Embedded Target for Virtual Platform and board [In the case of vHILS]
Image
Overflow of Embedded Target for Virtual Platform and board [In the case of evaluation board]

 

Features

  • Peripheral code is generated by adding blocks corresponding to the peripheral functions of the device to the model. The supported peripheral functions are as follows.  

    DevicesPeripheral functions
    RH850/U2B, RH850/F1KM-S1, RH850/F1KM-S4Port, ADC, CAN, UART, PWM
    R-Car S4, R-Car V4HGPIO, CAN, Ethernet
  • It automatically builds a vHILS verification environment using a virtual environment and enables verification of the cooperation between Simulink® and the virtual environment.
  • A comparison of vHILS and the Model In the Loop Simulation (MILS) execution results enables back-to-back testing as recommended by ISO 26262.
  • Embedded Target for RH850/F1KM Virtual Platform and board V2.01.00 works with the following tools to generate RTE, BSW, and MCAL code that conforms to the AUTOSAR specification. 
     - MICROSAR, DaVinci Developer, DaVinci Configurator Pro by Vector
     - MCAL by Renesas
  • Embedded Target for RH850/F1KM Virtual Platform and Board V2.01.00 supports verification not only in a virtual environment but also on an evaluation board using the E2 Emulator. 

All trademarks are the property of their respective owners.

Release Information

Latest Ver.: V2.01.00
Released: Dec 05, 2025
Release information (See Tool News)
Operating Environment

Type of License

Annual license, i.e. a license with a one-year expiry period. Contact your nearest Renesas distributor with regard to purchasing products.

For customer who consider commercial version of this tool

We recommend that you check operating environments of this tool carefully and try the free evaluation version (limited 3 months usage) on your development environment first to check if it works properly. In particular, you will also need to prepare partner tools, so please check the operating environments.

Evaluation Version Information

After obtaining this tool from the download list, please request the license key from your distributor or our sales representative, or follow the steps below.

  1. Access technical support on the Renesas Web site.
  2. Click on [LOG IN] and log in to the site with your ID which has been registered with My Renesas.
  3. Click on [SUBMIT A TICKET] in the upper right of the screen.
  4. Issue a new ticket by referring to the table and examples of entry which are shown to the right side.
    Title: Request a License Key for Evaluation version of the Embedded Target for [RH850 or R-Car] Virtual Platform
    Product Family: Target device using this tool (RH850/F1KM, etc.)
    Description: Describe the purpose for use, field of application for Embedded Target and your previous experience in using model-based development environments including MATLAB® and experience (or plans)  for using our target device.

Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.

Target Devices

Type Title Date
Software & Tools - Other
Log in to Download ZIP 21.88 MB
Software & Tools - Other
Log in to Download ZIP 11.24 MB
Software & Tools - Other
Log in to Download ZIP 8.51 MB
3 items
Type Title Date
Tool News - Release PDF 1.01 MB 日本語
Embedded Target for RH850 Virtual Platform is a development environment that generates peripheral code for target devices from Simulink models and enables cooperative verification as Virtual Hardware In the Loop Simulation (vHILS) in a virtual environment with Simulink.Embedded Target for RH850 Virtual Platform and Board is a development environment that generates peripheral code for target devices from Simulink models, enabling both vHILS and device verification using evaluation boards.This document describes the functional enhancements for this product for the RH850/F1KM.
Tool News - Release PDF 231 KB 日本語
Flyer PDF 654 KB 日本語
Tool News - Release PDF 303 KB 日本語
4 items

Collaboration

The cooperative environment will be provided by the partners. Please contact the following partners for purchase information.