Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Topics
・Embedded Target supports the new device RL78/F25.

We offer the above tool for co-simulation between the CS+/e² studio integrated development environment from Renesas interlinked with MATLAB® and Simulink® from the MathWorks, Inc. Among other things, this will support the validation of algorithms and model-based development by customers. For more information of this tool related to using evaluation version or purchasing commercial version, please refer to the release information.

Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.

Features

  • Generation of code for verifying algorithms from Simulink models
  • Automatic generation of Processor in the Loop Simulation (PILS) environments
  • Supported MCU families: RA, RX, RL78
  • What Customers Will be able to Do: Verify the functionality of code for target devices/Measure the performance of code for target devices
  • Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
  • Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
  • Learn More

Release Information

Latest Ver: V6.10.00
Released: Mar 20, 2026

For customer who consider commercial version of the Embedded Target

The Embedded Target is a tool that works with multiple software tools in tandem. 
This tool may not work properly under the following conditions.

  • MATLAB® versions are not supported by this product.
  • Specifications of Renesas MCU (such as small ROM/RAM size)
  • When a size of generated codes, which are affected size and complexity of the Simulink® model, is larger than ROM size of the MCU.
  • Inability to communicate due to network security settings, etc.

Again, please check operating environments of the Embedded Target carefully.

Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.

Target Devices

Target Devices

Note

Type Title Date
Upgrade - IDE
Log in to Download ZIP 18.25 MB
Upgrade - IDE
Log in to Download ZIP 867.85 MB 日本語
Upgrade - IDE
Log in to Download ZIP 1,770.53 MB 日本語
Upgrade - IDE
Log in to Download ZIP 1,835.27 MB 日本語
Upgrade - Compiler
Log in to Download ZIP 6.95 MB 日本語
5 items
Type Title Date
Flyer PDF 316 KB 日本語 , 简体中文
Manual - Development Tools PDF 441 KB 日本語
The release note for Embedded Target V6.10.00 provides information on operation environments, functional improvements and modifications in this version and usage limitations and precautions. Please read it carefully before using Embedded Target.
Manual - Development Tools PDF 7.16 MB 日本語
This manual describes how to use Embedded Target V6.10.00.
Tool News - Release PDF 140 KB 日本語
This document is Toolnews which provides information on the latest revision update for Embedded Target. It outlines Embedded Target versions need to be updated, summaries of release note including the improvements and changes by updating, and explainations the procedures for applying the update.
Quick Start Guide PDF 3.51 MB
This document describes how to install ‘Model-Based Development Environment for RA, RL78, RX Family [Embedded Target]’ and run demo models. Renesas Electronics offers Embedded Target for co-simulation between the CS+ integrated development environment from Renesas interlinked with MATLAB® and Simulink® from MathWorks, Inc. Embedded Target facilitates algorithm verification in embedded system models by automatically generating a test environment for Processor-in-the-Loop (PIL) simulation.
Tool News - Notification PDF 120 KB 日本語
This Tool News announcement provides information regarding the discontinuation of order acceptance for the model-based development environment for the Renesas RA, RL78, RX Family [Embedded Target] commercial license. It includes details on the end of order acceptance schedule and the licenses affected.
Tool News - Release PDF 183 KB 日本語
Tool News - Release PDF 53 KB 日本語
Tool News - Release PDF 68 KB 日本語
Tool News - Release PDF 54 KB 日本語
Tool News - Release PDF 44 KB 日本語
Tool News - Notification PDF 163 KB 日本語
12 items

Functionality

  • Generation of code for verifying algorithms from Simulink models
  • Automatic generation of Processor in the Loop Simulation (PILS) environments
  • Supported MCU families: RA, RL78, RX

What Customers Will be able to Do

  • Verify the functionality of code for target devices and
  • Measure the performance of code for target devices

Other Benefits to Customers

  • Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
  • Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
Image
em-concept-en

Software License Agreement

Software License Agreement (PDF | English, 日本語)