Overview
Description
Select the Form of License That Suits Your Pattern of Development
You can choose following types of Renesas compiler license listed in the following table for your development.
You can use a compiler product free of charge to evaluate its functions and performance before purchasing it.
See this page for the details of the free evaluation editions >>
Learn More
FAQ
| Title |
|---|
| What should I install to build environment with Floating License? |
| Checking Expiration Date of Annual Licenses |
| Applying Purchased License to Evaluation Edition (CC-RL/CC-RX/CC-RH) |
Target Devices
Videos & Training
Get started by learning how to set up and use a floating license for Renesas compilers, including CC‑RL, CC‑RX, and CC‑RH. The tutorial walks through the licensing process step by step, helping developers manage shared licenses smoothly across multiple environments. A great fit for teams aiming to optimize compiler usage and streamline development workflows.
News & Blog Posts
Blog Post Aug 5, 2022 |
Additional Details
Compiler License Types
| Attribute | Licenses | Description |
|---|---|---|
| Step1 Form of PCs usage | Node-Locked license |
|
| Floating license |
| |
| Step2 Features | Professional edition |
|
| Standard edition |
| |
| Step3 Period | Annual license |
|
| Permanent license |
| |
| Upgrading | Upgrade (edition) license |
|
| Upgrade (version) license |
|
Node-Locked License and Floating License
Node-Locked License
- These licenses allow you to use a compiler on one specific PC per license.
Floating License
- The licenses for the software are managed on a server, and are available for use on the PCs connected to a network within the range of the number of licenses.
- A license is available while a PC is connected with the server on the network.
- To use the license while disconnected from the network that includes the license server, customers can hold the license for a fixed period (as a number of days up to 99). Once the period which has been specified with the client elapses, the held license expires.
- The license resides on a client PC for 30 minutes after it is obtained at the start of building. If building has not finished after the 30 minutes have elapsed, the client PC retains the license for another 30 minutes. This cycle is repeated until building is finished.
Professional and Standard Edition
Professional edition
In addition to the features of the Standard editions, the Professional editions provide advanced features which help to improve the quality of your programs and shorten development periods. See the table below for the features and the supported compilers. Refer to Renesas Compilers Professional Editions (PDF | English, 日本語) for details of the features. You can refer to the Tool News for each of the features from the links in the table.
Standard edition
The Standard editions support C programming language specifications which comply with ANSI standards. These editions combine the basic features which are necessary for writing embedded programs with strong optimization functionality.
Additional Features of Professional Edition
| Features of the Professional Edition | Document | CC-RL | CC-RX | CC-RH |
|---|---|---|---|---|
| Checking of source code against MISRA-C: 2004/2012 rules (Note) | description | lens | lens | lens |
| Detection of stack smashing | description | lens | lens | lens |
| Enhanced security for dynamic memory management functions | description | lens | lens | lens |
| Function to detect illegal indirect function calls | description | lens | lens | lens |
| Half-precision floating-point | description | — | — | lens |
| Synchronization function working when control registers are updated | description | — | — | lens |
lens Supported | — Support is not planned.
Notes
- MISRA C is a set of guidelines developed by a non-profit organization, the Motor Industry Software Reliability Association (MISRA), regarding the reliability of software in the C programming language, particularly that for use in the automotive industry. More than 100 rules are set as guidelines regarding code in the C language. These rules are called MISRA C rules.
- "MISRA" and the triangle logo are registered trademarks of HORIBA MIRA Ltd, held on behalf of the MISRA Consortium.
Annual License and Permanent License
Annual license
- An annual license is valid for one year. The valid period is one year from initial registration with the Renesas Web site of the license acquisition code which accompanies the compiler product.
- This license becomes valid after a license key is acquired by registering the license acquisition code with the Renesas Web site. (Note1)
- The price of an annual license is lower than that of a permanent license.
- Annual licenses are useful in terms of flexibility in response to varying numbers of users in your team over time.
Permanent license
- No limit applies to the period of use for permanent licenses.
- A permanent license is made effective by registering the license key that accompanies the compiler product.
Note
- To acquire the license key which is required to use a compiler product, select [Obtaining a Subscription License Key] from the menu shown after logging-in to My Renesas and register the license acquisition code which is included with the compiler product.
Upgrade (edition) License
If you have a node-locked license for a standard edition, you can upgrade from the standard edition to a professional edition by additionally registering an Upgrade (edition) License.
Note that floating licenses and annual licenses cannot be upgraded in this way. This form of upgrade is only available for node-locked licenses.
Upgrade (version) License
The compiler licenses differ with the version. For example, V1.**.** and V2.**.** have different licenses since they are different versions.
In case of a license for an old version, you can use a new version of the compiler at low cost by additionally registering a Upgrade (version) License.
These licenses allow you to use both the new and old versions of a compiler.
This form of upgrade does not apply to annual licenses.
Applicable Compilers and Minimum Required Version for Compiler License
| Applicable MCUs | Product name | Compiler name | Minimum required version of compiler license | ||||
|---|---|---|---|---|---|---|---|
| Standard and Professional edition | Annual license | Floating License | Upgrade (edition) License | Upgrade (version) License | |||
| RL78 | C Compiler Package for RL78 Family | CC-RL | V1.01.00 | V1.01.00 | V1.01.00 | V1.01.00 | — |
| RX | C/C++ Compiler Package for RX Family | CC-RX | V2.04.00 | V2.03.00 | V2.03.00 | V2.04.00 | V3.00.00 |
| RH850 | C Compiler Package for RH850 Family | CC-RH | V1.03.00 | V1.02.00 | V1.02.00 | V1.03.00 | V2.00.00 |
Evaluation Edition
Before purchasing a compiler license, you can use an evaluation edition free of charge for evaluating the features and performance of the compiler product.
- During the trial period, you can use not only the standard edition (with basic features for embedded programs) without restrictions but also the professional edition (with advanced features for improving the efficiency of development).
- The trial period is the 60 days from the day the first build is executed after installing an evaluation edition.
Points of difference between usage within and after the trial period
| Compiler | Item | Evaluation edition (within the trial period) | Evaluation edition (after the trial period) | After purchasing a license |
|---|---|---|---|---|
| CC-RX | Commercial usage | — | — | lens |
| Standard edition (basic features) | lens | Restrictions on the linkage size Note1 | lens | |
| Professional edition (advanced features) | lens | — | lens Note3 | |
| Technical support (contact) | — | — | lens | |
| CC-RL CC-RH | Commercial usage | lens Note2 | lens | lens |
| Standard edition (basic features) | lens | [CC-RL] Note1 V1.11.00 or earlier versions: Restrictions on the linkage size V1.12.00 or later versions: Restrictions on the level of optimization [CC-RH] Note1 V2.07.00 or earlier versions: Restrictions on the linkage size V2.08.00 or later versions: Restrictions on the level of optimization | lens | |
| Professional edition (advanced features) | lens | — | lens Note3 | |
| Technical support (contact) | — | — | lens |
lens Available | — Not available
Note:
- After the trial period has expired, the linkage size or optimization will be restricted.
- Restrictions on the linkage size
CC-RL (V1.11.00 and earlier versions): no more than 64 KB, CC-RX: no more than 128 KB, CC-RH (V2.08.00 and earlier versions): no more than 256 KB - Restrictions on the level of optimization
CC-RL (V1.12.00 and later versions): The only selectable level of optimization is -Onothing (debug precedence) or -Olite (partial optimization).
CC-RH (V2.08.00 and later versions): The only selectable level of optimization is -Onothing (optimization with debugging precedence) or -Odefault(optimization that does not affect debugging)
- Restrictions on the linkage size
- The CC-RL and CC-RH are available for use in commercial purposes regardless of whether you have a license or not. However, you cannot use the features which are only available during the trial period for commercial purposes. If you will be using the CC-RL or CC-RH beyond the restrictions on the linkage size or optimization or would prefer to use the professional edition for commercial purposes, consider purchasing a compiler license.
- If you intend to use the features of the professional edition, consider purchasing the license for the professional edition.
Software License Agreement
Latest version
CC-RX V3.06.00 or later, CC-RL V1.13.00 or later, and CC-RH V2.06.00 or later
| Licenses | Software License Agreement | |
|---|---|---|
| Node-Locked License | annual | Software License Agreement LLWEB-20179381 |
| permanent | ||
| Floating License | annual | |
| permanent |
Previous version
CC-RX V3.05.00 or earlier, CC-RL V1.12.01 or earlier, and CC-RH V2.05.00 or earlier
| Licenses | Software License Agreement | |
|---|---|---|
| Node-Locked License | annual | Software License Agreement *IDF-16-015635 |
| permanent | Software License Agreement *IDF-15-015427 | |
| Floating License | annual | Software License Agreement *IDF-16-015637 |
| permanent | Software License Agreement *IDF-15-005414-01 |
Support
Support Communities
- CC-RX compiler license and IEC61508 kit
Hi everybody, We are going to buy a license for "CC-RX V3 compiler" (order code RTCRX0000CP03WNR) and "IEC61508 certification kit" (order code RTCRX0000TC03ZNR). I have a couple of questions: 1. Does the "IEC61508 certification kit" require mandatory to have a CC-RX license to operate? 2. The selected CC ...
Feb 20, 2024 - Compiler license for cloud compilation
Hi, As I couldn't find useful info elsewhere: Our company would like to use docker containers in the cloud for our compile process but we are unsure about what license would fit for that use-case as we would like to dynamically spawn multiple compile processes in parallel. We ...
Jul 11, 2024 - CCRX compiler license
... this message: W0561016:The evaluation version is valid for the remaining 1 days. Is my license valid for the new version? How do I update so that the warning goes away and I can continue to work? I know I can revert to the old compiler but would rather not.
Sep 24, 2020
Knowledge Base
- Is the RL78 C compiler license bought with CS+ valid for e² studio, too?
... into e² studio using the current license. For example, if the compiler supplied with CS+ was V1.01.00, then all V1.X RL78 C compiler versions (e.g. V1.01.00, V1.02.00, ...) can be integrated into e² studio using the current valid licenses. How to add toolchain ...
May 7, 2024 - Node Locked Compiler License Key in a Floating License Environment
No, node locked license keys are not convertible into Floating Licenses.
Dec 14, 2016 - Different C/C++ Compiler Licenses for RX Family
The supported core is different depending on the version. CC-RX V1: RXv1 core CC-RX V2: RXv1 core, RXv2 core CC-RX V3: RXv1 core, RXv2 core, RXv3 core "CC-RX V1" can be used for the development of a MCU equipped with the RXv2 core. However, note that ...
Feb 1, 2019