Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Features

  • Universally compatible pin out and command set
  • Low Sleep power for bootloader tasks
  • Standard block architecture with added 256-byte page erase for energy efficient Data Logging

Description

The AT25DF021A is a member of our System Enhancing class of code and data storage solutions. It is designed for all system memory tasks ranging from boot/code shadowing to data logging and includes the 256-byte page Erase feature that enables efficient, lower energy datalogging.

Parameters

AttributesValue
Memory ClassStandard Flash
Memory Density2
Operating Voltage Range (V)1.7 - 3.6
Speed85 MHz, 104 MHz
InterfaceSingle, Dual SPI
Temp. Range (°C)-40 to +85°C, -40 to +125°C
Deep Power Down (µA)0.2
Read Current (mA)4.5
Key BenefitFast read, Wide voltage

Package Options

Pkg. TypePkg. Dimensions (mm)Pitch (mm)
DFN2 x 30.5
DFN5 x 61.27
DWF——
SOIC 150MIL 8S1 8——
SOIC-N3.81 x 4.801.27
Part NumberStatusLongevityStockPackageBudgetary Price (USD)Sample CatalogCarrier TypeMoisture Sensitivity Level (MSL)Country of AssemblyCountry of Wafer Fabrication
AT25DF021A-DWFHTActive2034 JanOut of StockDWF<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>1
AT25DF021A-MAHN-TActive2034 JanIn StockDFN1ku | $0.74<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>Tape & Reel1TAIWANTAIWAN
AT25DF021A-MAHNHR-TActive2034 JanIn StockDFN1ku | $0.8<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>Tape & Reel1TAIWANTAIWAN
AT25DF021A-MHN-TActive2034 JanIn StockDFN1ku | $0.86<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>Tape & Reel1TAIWANTAIWAN
AT25DF021A-MHN-YActive2034 JanIn StockDFN1ku | $0.86<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>Tray1TAIWANTAIWAN
AT25DF021A-SSHN-BActive2034 JanOut of StockSOIC-N1ku | $0.47<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>Tube1PHILIPPINES, TAIWANTAIWAN
AT25DF021A-SSHN-TActive2034 JanIn StockSOIC-N1ku | $0.47<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>Tape & Reel1PHILIPPINES, TAIWANTAIWAN
AT25DF021A-SSHNHR-BActive2034 JanOut of StockSOIC 150MIL 8S1 8<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>3
AT25DF021A-SSHNHR-TActive2034 JanIn StockSOIC-N1ku | $0.83<a href="https://www.renesas.com/samplecomponents/scripts/samplecenter/adestotech?cmd=menu" title="Request Samples" rel="noreferrer">Request Samples</a>Tape & Reel1PHILIPPINESTAIWAN
AT25DF021A-XMHN-BNRND2034 JanOut of StockTSSOP1ku | $0.69Tube1PHILIPPINESTAIWAN
AT25DF021A-XMHN-TNRND2034 JanIn StockTSSOP1ku | $0.69Tape & Reel1PHILIPPINESTAIWAN
AT25DF021A-XMHNHR-TNRND2034 JanIn StockTSSOP1ku | $0.99Tape & Reel1PHILIPPINESTAIWAN

Support Communities

  1. Flash Memory AT25DF021A-UUNHR-T

    During the design phase in which I find myself, I cannot find anywhere the footprint of the relevant component as mentioned above. I notice that on Page 8 of that datasheet, I find that the TOP VIEW is strangely different from the TOP VIEW on Page 57. I kindly ask ...

    Sep 14, 2024
  2. Using DA14531MOD SPI flash to store bonding database

    Hello, If USER_CFG_APP_BOND_DB_USE_SPI_FLASH is defined, then I can see in app_bond_cb.c that it will use SPI flash to store the bonding database. Can the SPI flash in the DA14531MOD be used for this purpose and if so, where in the ...

    Feb 4, 2023
  3. DA14531 (WLCSP17) Cannot flash external SPI (or read OTP) - Failed clearing memory address 7FC3C08. Failed configuring SPI ports and pins.QuestionContext

    Question How can we let SmartSnippets Toolbox turn off HW_RESET, or otherwise customize the jtag_programmer.bin ? Context We have been able to run our firmware (based on the ble_app_example, for SDK version: 6.0.14.1114) using Keil - so we know we can program the RAM ...

    Mar 21, 2023
View All Results from Support Communities (6)