Overview
Description
The ZSSC3286 evaluation kit provides the hardware needed for the configuration, calibration, and evaluation of the ZSSC3286 sensor signal conditioner (SSC) IC. A user's PC can communicate with the ZSSC3286 IC socketed on the ZSSC3286 evaluation board via USB and IO-Link, using the included RH4Z2501-PMOD board (IO-Link physical layer transceiver board with Pmod™ interface) and the 2-channel IO-Link master. Furthermore, the ZSSC3286 evaluation kit contains the SSC communication board for configuration via I²C.
The evaluation kit software is available online for free download.
To enable product comparisons, this modular kit is compatible with other selected Renesas devices. Contact your local sales representative for more information.
Kit Contents
The ZSSC3286 evaluation kit is an all-in-one evaluation system for designing IO-Link sensing applications. The following components are included:
- ZSSC3286 evaluation board
- SSC communication board
- SSC sensor replacement board
- CCE4510 IO-Link master board
- RH4Z2501-PMOD board
- ZSSC3286 samples (5 pcs.)
- USB and IO-Link cables
- Tweezers
- Software, including ZSSC3286 IO-Link Device Description (IODD) generator
Features
- All-in-one starter kit
- Full connectivity chain from the sensor to the USB port
- Functional evaluation of the ZSSC3286 SSC via the IO-Link and I²C interfaces
- Sensor configuration and calibration
- ZSSC3286 firmware updates
Applications
Design & Development
Videos & Training
See how the ZSSC3286 sensor signal conditioner combines a dual path analog front-end with an integrated IO-Link stack supporting the Smart Sensor Profile in COM3 mode. The demonstration highlights the full-chain evaluation kit featuring the ZSSC3286 evaluation board and RH4Z2501-PMOD, enabling sensor signal conditioning evaluation and development.
News & Blog Posts
Support
Support Communities
- ZSSC328x application
There was a video that demonstrate how to work with the ZSSC328X application with ZSSC328x developement kit. Anobody what is the link to this video?
Aug 2, 2025
Knowledge Base
- IODD Generator
The Evaluation Kit comes with a GUI to configure and evaluate the device. The GUI has an integrated IODD generator.
Oct 16, 2024 - Compatible IO-Link Master
The ZSSC3286 Evaluation Kit already contains a 2 channel IO-Link master for evaluation. All needed cables and connectors are part of the Kit.
Oct 16, 2024 - Configuration and Programming
The ZSSC3286 has all hardware and firmware components integrated. There is no software development needed. The device must be configured according to your application. This configuration can be done with the GUI coming with the Evaluation Kit.
Oct 16, 2024