Skip to main content
Renesas Electronics Corporation

Overview

The ZMID4201STKIT is an all-in-one starter kit, providing fully-functional evaluation of the ZMID4200 position sensor. This kit combines the linear, rotary, and arc types into a single kit, along with the communications board required to interface with the control software. This evaluation kit allows to select the wanted interface among Analog (default), PWM or SENT.

Features

  • ZMID-COMBOARD communications board
  • ZMID4200 linear application module
  • ZMID4200 rotary application module
  • ZMID4200 arc application module
  • Micro B USB Cable
  • 2 x interface cables

Products in the Design

Sample & Buy

ZMID-COMBOARD Communications Board

Absolute arc with 130-degree range

ZMID4200STKIT Not Recommended for New Designs
Pb (Lead) Free:Yes
1u | $149.00Budgetary Price