Skip to main content
Renesas Electronics Corporation

Overview

The Renesas Starter Kit for RX62T is intended as a user-friendly introductory and evaluation tool for the RX62T microcontroller. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using High-performance Embedded Workshop.

The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run only minutes from opening box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.

Products in the Design

Sample & Buy

Renesas Starter Kit for RX62T

Renesas Starter Kit for RX62T (Kit with HEW)

R0K5562T0S900BE Last Time Buy
Description:Renesas Starter Kit for RX62T (Kit with HEW)
Debugger supplied:None
1u | $176.47Budgetary Price

Videos & Training

Support

Support Communities

  1. RX62T starter kit button enable

    Hello Everyone, I am trying to use the button on my RX62T starter kit to turn one LED. My code is below and isnt properly functioning. Can anyone please help me? thank you very much! #include int main(){ PORT7.DR.BIT.B1 = 0 ; // Make LED0 ...

    Dec 5, 2017
  2. RX62T (Starter kit) doesn´t load new programm

    Hello all, we have a small problem with loading new programs on our Renesas RX62T. We build a new program and debug (Hardware debug) it without any fail massage. But the Renesas start only the old program. We delete the old program from e2-Studio and also Reset or restart ...

    Feb 3, 2020