Overview
Description
The Renesas Starter Kit for RX610 is intended as a user-friendly introductory and evaluation tool for the RX610 microcontroller. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using High-performance Embedded Workshop as well as programming the device using E1 emulator and/or Flash Development Toolkit.
The Renesas Starter Kit for RX610 may be connected to the host PC using a simple RS232 serial connection or via the included USB E1 on chip debugging interface.
The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run only minutes from opening box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.
Applications
Design & Development
Videos & Training
Additional Videos
Support
Support Communities
- about simple code in c for microcontroller
can anybody help me??I want simple code using c to help me for understanding how i can use registers to transfer data on specific portthe example about anything likepush button when I pressed on it the led flashed
Dec 31, 2010