Overview
The Renesas Starter Kit for RX113 is intended as a user-friendly introductory and evaluation tool for the RX113 microcontroller. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using CS+.
The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run only minutes from opening box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.
* In order to make a product installer active, this product needs the Internet environment.
* CS+ is not generally promoted to the U.S. and European customers. Customers in the U.S. and Europe who are interested in CS+ are requested to contact our regional marketing departments for details.
Features
- Renesas microcontroller programming
- User code debugging
- User circuitry such as switches, LEDs, and a potentiometer
- Sample application
- Sample peripheral device initialization code
Sample & Buy
Renesas Starter Kit for RX113 (Kit with CS+)
| Description: | Renesas Starter Kit for RX113 (Kit with CS+) |
| Debugger supplied: | None |
Videos & Training
Additional Videos
Support
Support Communities
- Using Renesas Flash Programmer with RX113 Starter Kit
Hi!I want to use the Renesas Flash Programmer with the RX113 Starter Kit to donwload my program.As far as I understand, I simply must put the MCU from Single Chip Mode to USB Boot Mode by setting SW4 to ON/ON, so that MD and UB (P14 ...
May 13, 2024 - Using Renesas Flash Programmer with RX113 Starter Kit
Hi!I want to use the Renesas Flash Programmer with the RX113 Starter Kit to donwload my program.As far as I understand, I simply must put the MCU from Single Chip Mode to USB Boot Mode by setting SW4 to ON/ON, so that MD and UB (P14 ...
May 13, 2024 - RX113 Second Gen Kit - water tolerance
Hi All, I have RX113 Starter kit (Y-RX113CAPT01). It says user can evaluate water tolarance with it. However I couldn't find any guidance/code examples on how to do it. Could anyone help with with it, please. John.
Oct 20, 2016