Skip to main content
Renesas Electronics Corporation

Overview

The QCIOT-MOTIONPOCZ board is an analog motion sensor that can detect motion from up to two meters away by using a passive infrared (PIR) sensor.

The sensor is connected to a bandpass filter using the SLG88103 operational amplifier to condition and filter the signal. The amplified condition signal is connected to the analog pin of the MCU to determine the strength and distance of motion. The signal also connects to nanopower comparators that form a window comparison to be used to wake up an MCU or system at motion detection.

The solution can be powered by either connecting an MCU board or with an external connection. The external regulator supports powering the MCU and other connecting solutions. This solution supports the QuickConnect IoT (QCIOT) ecosystem. Other solutions can be daisy chained.

Features

  • Operating voltage: 5V to 16V
  • Sensor current: ~13µA
  • Operational current: ~19µA
  • Always on autonomous operation

Products in the Design

SLG59M1639V
5.5V, 45mΩ, 2A Dual-Channel Load Switch with Reverse Current Blocking
ISL28915
Nano Power, Push/Pull Output Comparator

Sample & Buy

QCIOT-MOTIONPOCZ Motion Sensor Board - Top

Motion Sensor QuickConnect IoT Module Board

QCIOT-MOTIONPOCZ Active

Add-on Hardware

Additional boards that work with this platform. Some may be required for full functionality or to evaluate specific features.

Trail Camera Reference Kit

Showcase low‑power vision AI and fast‑boot Linux using a trail camera demo built on the RZ/V2L platform.

Support

Support Communities

  1. RZG2L Fast Boot Optimization Help Needed – Thermal Application Visible on OLED Only After 14s Despite systemd Showing <10s Boot Time

    Hello Everyone, We are working on a thermal imaging application on a Renesas RZG2L and are trying to reduce the complete boot-to-display time of our application to below 10 seconds. Our application is started using thermal.service, which launches a thermal imaging binary during boot. Currently, the application ...

    May 12, 2026
  2. Deep Sleep Mode in A55 (RZV2L)

    Hi Team,  We are using RZ/V2L based customized board, and we are exploring the possibility of enabling a deep sleep mode for the A55 core (running Linux), keeping only the M33 core active to maximize battery life. Any feasibilities done on this, will it be possible to achieve ...

    Jun 17, 2025