Skip to main content
Renesas Electronics Corporation

Renesas’ Timing product portfolio has been acquired by SiTime.

Datasheets, documentation, and sample orders remain available on Renesas.com through late 2026. For new designs, purchasing, support, and product inquiries, visit SiTime.com or send an email to [email protected]. Full transition to SiTime is expected by late 2026.

Alternative(s) Available

Overview

The VersaClock® 3S-5P3502x programmer board is made to ease the programming of blank 5P35021 and 5P35023 devices. With the on-board USB interface, the Renesas Timing Commander™ graphical user interface (GUI) is used to communicate with the blank device in the socket for configuration and programming.

Features

  • Program VersaClock 3S – 5P3502x blank parts in the socket
  • Removable socket board
    • EVK5P35021PROG is a VersaClock 3S USB programmer board with a QFN20 socket board for the 5P35021 device
    • EVK5P35023PROG is a VersaClock 3S USB programmer board with a QFN24 socket board for the 5P35023 device
  • Programmer board is powered by USB port
  • Programmer board uses Renesas Timing CommanderTM GUI to program the blank parts
  • USB port is the communication channel between the GUI and the VersaClock 3S–5P3502x device in the socket

Products in the Design

Sample & Buy

Applied Filters: