Skip to main content
Renesas Electronics Corporation

Overview

The DA14AVDDECTDEVKT is a development kit for the DA14AVDDECT Audio Voice Data module. This module is a member of the wireless module family, operating on the interference free DECT frequency band (1.9GHz) and it can be used in hosted or embedded audio, voice and data (AVD) applications. There are three stacks available for the AVD module, falling into two categories, the Audio Data (AD) stacks (Tour Guide stack and Public Address stack) and the Voice Data (VD) stack.

The development kit has the AVD module mounted on carrier boards. The carrier board has an Arm® debug interface and a USB-UART interface for programming and debugging the AVD module. The development kit also has some pre-defined push buttons and LEDs tailored for the example applications, Li-ion battery connectors, and 3.5mm audio jacks. This development kit targets users who are familiar with application-level software programming and does not require detailed understanding of the DECT protocol.

The DA14AVDDECTDEVKT development kit for the DA14AVDDECT module is the ideal starting point for developing complete voice or audio applications of any size. It includes all the hardware and points users to the software and documentation for a basic system that will let them explore the module’s potential for their target application.

Features

  • Next-generation DECT radio performance:
    • Multi-level modulation
    • Zero blind slot support
  • Extensive processing power
  • Hi-Fi audio support
  • Integrated antenna and support for optional external antenna
  • Battery management with charger and fuel gauge
  • Choice of voice and data or audio and data software stacks

Products in the Design

Sample & Buy

DA14AVDDECTDEVKT

Active
MOQ:1
SPQ:1
Pb (Lead) Free:Yes
Pkg. Type:Box
Carrier Type:Box
Assembly Location:GERMANY
1u | $393.00Budgetary Price

Support

Support Communities

  1. Regarding the DA14AVDDECTDEVKT question:

    Currently, our design requires enabling SPI and the second UART. I reviewed the API HAL Device Control section in the wampa4985pp_api documentation, which mentions "See SC14441 data sheet." However, I couldn't find this document online. Could you please advise on how I can obtain it? Or, how can ...

    Apr 23, 2025
  2. DA14AVDDECTDEVKT

    Hi, In the User Manual UM-D-012 from the DA14AVDDECTDEVKT there are references to the UM-D-011, DA14AVDDECT Production Programming abd Configurarion Manual, but it is not supplied with the developnent kit. Any one knows where or who can provide this? Best, Pere [locked by: GG_Renesas at ...

    Jun 16, 2023
  3. DA14AVDDECTDEVKT

    Hi, I'm trying to develop a DECT intercom system as described in the CVM stack on the DA14AVDDECTDEVK, but in a stereo mode. There is a way to implement it in the conference CVM mode? Best, Pere

    Oct 8, 2022
View All Results from Support Communities (8)