Skip to main content
Renesas Electronics Corporation

Description

The Production Line Tool (PLT) helps increase throughput in volume testing and programming of units centered around Renesas Bluetooth ICs.

In the PLT, the Golden Unit (GU) is a daughterboard mainly used for various purposes, including:

  • RF transmitter for the RF RSSI DUT test
  • RF receiver for the device Bluetooth Low Energy (LE) advertisement scan test
  • Audio tone generator for the audio test
  • Controlling the complex programmable logic device (CPLD)

The GU uses an SPI Flash memory mounted on the PLT board. The SPI Flash is pre-programmed with a specific production test firmware. If required, there are several methods for upgrading the GU firmware, including via the PLT’s GU JTAG connector or the UART. The latest GU firmware can be found inside the latest PLT software release, under the executables\binaries\GU folder.

Note: PLT v4.1 and onwards requires the latest firmware version of the Golden Unit. If the Golden Unit firmware is not updated, then the PLT applications will not run. The Golden Unit is calibrated during PLT production. It is delivered with a calibration characterization document.

Applications

Type Title Date
Manual - Development Tools PDF 10.15 MB
1 item

Software & Tools

Software & Tools

Software title
Software type
Company
Connectivity Production Line Tool
The Connectivity Production Line Tool (PLT) is a flexible platform that helps to increase throughput in volume tests and programming of units centered around Renesas Connectivity ICs.
Programmer (Unit/SW) Renesas
1 item
Part NumberStatusStockBudgetary Price (USD)Sampleable
DA14580 PLT Golden UnitActiveIn Stock1u | $150N/A