Overview
The DA14580 USB Dongle is an 802.15.1 Bluetooth® Low Energy dongle designed for use with the DA14580 Basic, Pro, or Expert Development Kits.
Sample & Buy
DA14580DONGLE
Active| MOQ: | 1 |
| SPQ: | 1 |
| Pb (Lead) Free: | Yes |
| Carrier Type: | Box |
| Temp. Range (°C): | -40 to +85°C |
| Assembly Location: | GERMANY |
Resources
Support
Support Communities
- How to update the software over the air (SUOTA) with the SmartSnippets ?
Hi,Dialog! I recently doing SUOTA, use a DA14580 device that external SPI FLASH as SUOTA Initiato, and the SmartSnippets v3.6. I have the following problems: 1.How to open the SmartSnippets with UART/SPI mode?Is the use of DA14580 Dongle? 2.Now I open the SmartSnippets ...
Jun 1, 2015 - SUOTA with DEVKIT-B
Hi Dialog, How to use DEVKIT-B as DA14580 USB Dongle ? Regards,
Sep 16, 2016 - DSPS: Wait after SPS_SERVER_ENABLE_CFM before sending data?
... there). What I want to do is to send data from the MSP430 to a Windows terminal over SPS: MSP430 --> DA14580 (DevKit Pro, SPS server) --> DA14580 (Dongle, SPS client) --> Terminal (PC) I noticed the following: After enabling the SPS service and receiving the SPS_SERVER_ENABLE_CFM message, I have ...
Apr 6, 2016