Overview
The DA14531-01FXDB-P is the FCGQFN24 daughterboard for the DA14531 Development Kit Pro's motherboard.
The DA14531-01 SmartBond TINY™ Development Kit Pro (DA14531-00FXDEVKT-P) is the ideal way to quickly and easily get started developing applications and products using the DA14531 Bluetooth® Low Energy (LE) system-on-chip (SoC).
Features
- Embedded printed antenna
- RF port output (connector not included)
- DA14531 power mode configuration switch (only for backward compatibility with DA1458x DK PRO motherboard)
- Current measurement port to connect external measurement equipment
- Onboard JTAG connector
- Support for coin cell battery (battery holder not included)
Sample & Buy
DA14531-01FXDB-P
Active| MOQ: | 1 |
| SPQ: | 1 |
| Pb (Lead) Free: | Yes |
| Carrier Type: | Box |
| Assembly Location: | GERMANY |
Add-on Hardware
SmartBond TINY DA14531 Bluetooth Low Energy 5.1 System-on-Chip Development Kit Pro
Resources
Support
Support Communities
- SPS do not compile / or crash with Eclipse in Linux
... the same address which is 000010fc. Please try to reproduce, I am sure that there is a bug here. This is what I am using: DA14531-00FXDEVKT-P with DA14531-01FXDB-P daughterboard. SDK 6.0.22.1401 PSP 6.150.6.77 Linux Mint 21.2 Thank you, Rémi
Aug 29, 2024 - SPS running but cannot connect as UART
Hi, With DA14531-00FXDEVKT-P and daughterboard DA14531-01FXDB-P I was able to compile the dsps_device project with Keil on a windows machine and to make it run in the debugger. I can detect the device with many Android apps but I did not get successful communication from ...
Aug 24, 2024 - SPS do not compile / or crash with Eclipse in Linux
... the same address which is 000010fc. Please try to reproduce, I am sure that there is a bug here. This is what I am using: DA14531-00FXDEVKT-P with DA14531-01FXDB-P daughterboard. SDK 6.0.22.1401 PSP 6.150.6.77 Linux Mint 21.2 Thank you, Rémi
Aug 29, 2024