Description
Returns the file list in a specified folder.
CAll (METHOD = GET)
http://tool-cloud2.renesas.com/system/api/?key=[API_KEY]&module=structure&action=list&project=[PROJECT_NAME]&path=[FOLDER_PATH]
PROJECT_NAME: Specify PROJECT_NAME obtained as project information.
FOLDER_PATH: Specify FOLDER_PATH obtained as path information. / indicates root.
Result
{
"structure": [
{
"path": "[OBJECT_PATH]",
"name": "[OBJECT_NAME]",
"type": "[OBJECT_TYPE]"
},
...
]
}
OBJECT_PATH: Indicates object path.
OBJECT_NAME: Indicates file or folder name.
OBJECT_TYPE: 1 in case folder, 2 in case file, null in case no file and folder.
Support
Support Communities
Get quick technical support online from Renesas Engineering Community technical staff.
Knowledge Base
Browse our knowledge base for helpful articles, FAQs, and other useful resources.