Overview
Description
Select the Form of License That Suits Your Pattern of Development
You can choose following types of Renesas compiler license listed in the following table for your development.
You can use a compiler product free of charge to evaluate its functions and performance before purchasing it.
See this page for the details of the free evaluation editions >>
Learn More
FAQ
| Title |
|---|
| What should I install to build environment with Floating License? |
| Checking Expiration Date of Annual Licenses |
| Applying Purchased License to Evaluation Edition (CC-RL/CC-RX/CC-RH) |
Target Devices
Videos & Training
Get started by learning how to set up and use a floating license for Renesas compilers, including CC‑RL, CC‑RX, and CC‑RH. The tutorial walks through the licensing process step by step, helping developers manage shared licenses smoothly across multiple environments. A great fit for teams aiming to optimize compiler usage and streamline development workflows.
News & Blog Posts
Blog Post Aug 5, 2022 |
Additional Details
Compiler License Types
| Attribute | Licenses | Description |
|---|---|---|
| Step1 Form of PCs usage | Node-Locked license |
|
| Floating license |
| |
| Step2 Features | Professional edition |
|
| Standard edition |
| |
| Step3 Period | Annual license |
|
| Permanent license |
| |
| Upgrading | Upgrade (edition) license |
|
| Upgrade (version) license |
|
Node-Locked License and Floating License
Node-Locked License
- These licenses allow you to use a compiler on one specific PC per license.
Floating License
- The licenses for the software are managed on a server, and are available for use on the PCs connected to a network within the range of the number of licenses.
- A license is available while a PC is connected with the server on the network.
- To use the license while disconnected from the network that includes the license server, customers can hold the license for a fixed period (as a number of days up to 99). Once the period which has been specified with the client elapses, the held license expires.
- The license resides on a client PC for 30 minutes after it is obtained at the start of building. If building has not finished after the 30 minutes have elapsed, the client PC retains the license for another 30 minutes. This cycle is repeated until building is finished.
Professional and Standard Edition
Professional edition
In addition to the features of the Standard editions, the Professional editions provide advanced features which help to improve the quality of your programs and shorten development periods. See the table below for the features and the supported compilers. Refer to Renesas Compilers Professional Editions (PDF | English, 日本語) for details of the features. You can refer to the Tool News for each of the features from the links in the table.
Standard edition
The Standard editions support C programming language specifications which comply with ANSI standards. These editions combine the basic features which are necessary for writing embedded programs with strong optimization functionality.
Additional Features of Professional Edition
| Features of the Professional Edition | Document | CC-RL | CC-RX | CC-RH |
|---|---|---|---|---|
| Checking of source code against MISRA-C: 2004/2012 rules (Note) | description | lens | lens | lens |
| Detection of stack smashing | description | lens | lens | lens |
| Enhanced security for dynamic memory management functions | description | lens | lens | lens |
| Function to detect illegal indirect function calls | description | lens | lens | lens |
| Half-precision floating-point | description | — | — | lens |
| Synchronization function working when control registers are updated | description | — | — | lens |
lens Supported | — Support is not planned.
Notes
- MISRA C is a set of guidelines developed by a non-profit organization, the Motor Industry Software Reliability Association (MISRA), regarding the reliability of software in the C programming language, particularly that for use in the automotive industry. More than 100 rules are set as guidelines regarding code in the C language. These rules are called MISRA C rules.
- "MISRA" and the triangle logo are registered trademarks of HORIBA MIRA Ltd, held on behalf of the MISRA Consortium.
Annual License and Permanent License
Annual license
- An annual license is valid for one year. The valid period is one year from initial registration with the Renesas Web site of the license acquisition code which accompanies the compiler product.
- This license becomes valid after a license key is acquired by registering the license acquisition code with the Renesas Web site. (Note1)
- The price of an annual license is lower than that of a permanent license.
- Annual licenses are useful in terms of flexibility in response to varying numbers of users in your team over time.
Permanent license
- No limit applies to the period of use for permanent licenses.
- A permanent license is made effective by registering the license key that accompanies the compiler product.
Note
- To acquire the license key which is required to use a compiler product, select [Obtaining a Subscription License Key] from the menu shown after logging-in to My Renesas and register the license acquisition code which is included with the compiler product.
Upgrade (edition) License
If you have a node-locked license for a standard edition, you can upgrade from the standard edition to a professional edition by additionally registering an Upgrade (edition) License.
Note that floating licenses and annual licenses cannot be upgraded in this way. This form of upgrade is only available for node-locked licenses.
Upgrade (version) License
The compiler licenses differ with the version. For example, V1.**.** and V2.**.** have different licenses since they are different versions.
In case of a license for an old version, you can use a new version of the compiler at low cost by additionally registering a Upgrade (version) License.
These licenses allow you to use both the new and old versions of a compiler.
This form of upgrade does not apply to annual licenses.
Applicable Compilers and Minimum Required Version for Compiler License
| Applicable MCUs | Product name | Compiler name | Minimum required version of compiler license | ||||
|---|---|---|---|---|---|---|---|
| Standard and Professional edition | Annual license | Floating License | Upgrade (edition) License | Upgrade (version) License | |||
| RL78 | C Compiler Package for RL78 Family | CC-RL | V1.01.00 | V1.01.00 | V1.01.00 | V1.01.00 | — |
| RX | C/C++ Compiler Package for RX Family | CC-RX | V2.04.00 | V2.03.00 | V2.03.00 | V2.04.00 | V3.00.00 |
| RH850 | C Compiler Package for RH850 Family | CC-RH | V1.03.00 | V1.02.00 | V1.02.00 | V1.03.00 | V2.00.00 |
Evaluation Edition
Before purchasing a compiler license, you can use an evaluation edition free of charge for evaluating the features and performance of the compiler product.
- During the trial period, you can use not only the standard edition (with basic features for embedded programs) without restrictions but also the professional edition (with advanced features for improving the efficiency of development).
- The trial period is the 60 days from the day the first build is executed after installing an evaluation edition.
Points of difference between usage within and after the trial period
| Compiler | Item | Evaluation edition (within the trial period) | Evaluation edition (after the trial period) | After purchasing a license |
|---|---|---|---|---|
| CC-RX CC-RH | Commercial usage | — | — | lens |
| Standard edition (basic features) | lens | Restrictions on the linkage size Note1 | lens | |
| Professional edition (advanced features) | lens | — | lens Note3 | |
| Technical support (contact) | — | — | lens | |
| CC-RL | Commercial usage | lens Note2 | lens | lens |
| Standard edition (basic features) | lens | V1.11.00 or earlier versions: Restrictions on the linkage size Note1 V1.12.00 or later versions: Restrictions on the level of optimization Note1 | lens | |
| Professional edition (advanced features) | lens | — | lens Note3 | |
| Technical support (contact) | — | — | lens |
lens Available | — Not available
Note:
- After the trial period has expired, the linkage size or optimization will be restricted.
- Restrictions on the linkage size
CC-RL (V1.11.00 and earlier versions): no more than 64 KB, CC-RX: no more than 128 KB, CC-RH: no more than 256 KB - Restrictions on the level of optimization
CC-RL (V1.12.00 and later versions): The only selectable level of optimization is -Onothing (debug precedence) or -Olite (partial optimization).
- Restrictions on the linkage size
- The CC-RL is available for use in commercial purposes regardless of whether you have a license or not. However, you cannot use the features which are only available during the trial period for commercial purposes. If you will be using the CC-RL beyond the restrictions on the linkage size or optimization or would prefer to use the professional edition for commercial purposes, consider purchasing a compiler license.
- If you intend to use the features of the professional edition, consider purchasing the license for the professional edition.
Software License Agreement
Latest version
CC-RX V3.06.00 or later, CC-RL V1.13.00 or later, and CC-RH V2.06.00 or later
| Licenses | Software License Agreement | |
|---|---|---|
| Node-Locked License | annual | Software License Agreement LLWEB-20179381 |
| permanent | ||
| Floating License | annual | |
| permanent |
Previous version
CC-RX V3.05.00 or earlier, CC-RL V1.12.01 or earlier, and CC-RH V2.05.00 or earlier
| Licenses | Software License Agreement | |
|---|---|---|
| Node-Locked License | annual | Software License Agreement *IDF-16-015635 |
| permanent | Software License Agreement *IDF-15-015427 | |
| Floating License | annual | Software License Agreement *IDF-16-015637 |
| permanent | Software License Agreement *IDF-15-005414-01 |
Support
Support Communities
- Compiler license needed for M3T-NC308WA ?
... using the CD that came with the product. It needs subject toolchain to program the MCU. I noticed the setup wants me to add a license key. However there is no license key that came with the package. Can someone please confirm if this needs an additional compiler license or ...
Aug 7, 2024 - Compiler license transfer from network to USB
Hello: In the past we have been big M16C users. Now we have moved on to RX and Synergy. We are still supporting some M16C products and now have a problem. We are retiring the server that hosts the M16C licenses and would like to move those licenses to USB ...
Oct 3, 2016 - How to get old CCRX compiler licenses
... on CCRX V.1 and V.2, which are still under maintenance and further development. Unfortunately, I am unable to find a way to purchase licenses for these older compiler versions. Could you please advise how I can legally obtain or continue to use CCRX V.1 and V.2 ...
Oct 7, 2025
Knowledge Base
- Is the RL78 C compiler license bought with CS+ valid for e² studio, too?
... into e² studio using the current license. For example, if the compiler supplied with CS+ was V1.01.00, then all V1.X RL78 C compiler versions (e.g. V1.01.00, V1.02.00, ...) can be integrated into e² studio using the current valid licenses. How to add toolchain ...
May 7, 2024 - Is RX C/C++ compiler license bought with CS+ valid for e² studio, too?
... the current license. For example, if the compiler supplied with CS+ (or CubeSuite+) was V2.00.01, then all V2.X RX C/C++ compiler versions (e.g. V2.01.00, V2.01.01, V2.02.00, ...) can be integrated into e² studio using the current valid licenses. How ...
Sep 4, 2015 - Node Locked Compiler License Key in a Floating License Environment
No, node locked license keys are not convertible into Floating Licenses.
Dec 14, 2016