Skip to main content
Renesas Electronics Corporation

Overview

Description

  • The practice of publishing separate e2 studio releases for Synergy has been discontinued. For SSP 2.0.0 and future SSP releases, users will be requested to use the Platform installer to install e2 studio and SSP together. The Platform installer for SSP 2.0.0 and future releases is available from the download page for SSP.
  • It is strongly recommended that users do not use the older versions of e2 studio for SSP 2.0.0 and future releases as these combinations have not been tested and are not supported.
  • For additional support or to request an older version of SSP or e2 studio for Synergy, users should submit a ticket through the Renesas Knowledge Base.

Target Devices

Support

Support Communities

  1. Switching from e2 Studio to IAR Embedded Workbench® for Renesas Synergy™

    For some time now, the Synergy Platform has had the IAR Embedded Workbench® for Renesas Synergy ™ development environment and compiler available to developers. Engineers that have been using e2 Studio might be hesitant to convert their e2 projects into IAR Workbench projects. Doesn’t this seem like it ...

    Jan 26, 2017
  2. Coming up to Speed with e2 Studio 5.2.1 New Features

    ... leave the remaining features to the reader to explore.   Figure 1 – New Features and the Benefits A great addition to the recent release is that e2 Studio now supports C++ (IAR Embedded Workbench for Renesas Synergy™ also has added support)! The support is compatible with the recent SSP 1 ...

    Feb 2, 2017
  3. Introducing the IAR Embedded Workbench® for Renesas Synergy™

    ... for Renesas Synergy™ which is now included in the Renesas Synergy™ Platform.   Developers using the Synergy Platform now have the choice to use E2 studio, an Eclipse based Integrated Solution Development Environment using GCC for ARM®, or IAR EW for Synergy with the IAR C/C ...

    Aug 11, 2016
View All Results from Support Communities (32)

Knowledge Base

  1. Command-line build of e² studio project

    ... command lineThe following manual explains about launch options of eclipsec.exe (or e2studio.exe) and the ini file: Eclipse Platform Help - Runtime optionsIn the projects for Renesas Synergy™ devices, add the following line in the eclipse.ini file (after the line -vmargs) :-Dcom.renesas.synergyLicenseFile= Mar 25, 2024

  2. Differences between e² studio and CS+ Integrated Development Environments

    ... studio, CS+. For more information, see the IDE Release Notes and the respective documentation. [Supported Device Families]e² studioCS+ (CS+ for CC) CS+ (CS+ for CA,CX) RX, RL78, RH850,RA, RZ, RE,Renesas Synergy™,RISC-V MCU RX, RL78, RH850 RL78, 78K, V850 [Supported Compilers]e² studio ...

    Oct 9, 2024
  3. GNU compilers for e² studio

    ... Software Support Package (Synergy SSP) can be selected at installation of e² studio  downloaded from the Renesas Synergy™ Platform site.  Please visit Renesas Synergy™ Platform - Development tools for the details about Synergy SSP. [RZ family]  “GNU ARM Embedded Toolchain” is freely available (see Note 2) for e² studio ...

    Apr 8, 2019
View All Results from Knowledge Base (5)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?