Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

  • The practice of publishing separate e2 studio releases for Synergy has been discontinued. For SSP 2.0.0 and future SSP releases, users will be requested to use the Platform installer to install e2 studio and SSP together. The Platform installer for SSP 2.0.0 and future releases is available from the download page for SSP.
  • It is strongly recommended that users do not use the older versions of e2 studio for SSP 2.0.0 and future releases as these combinations have not been tested and are not supported.
  • For additional support or to request an older version of SSP or e2 studio for Synergy, users should submit a ticket through the Renesas Knowledge Base.

Target Devices

Support Communities

  1. Switching from e2 Studio to IAR Embedded Workbench® for Renesas Synergy™

    For some time now, the Synergy Platform has had the IAR Embedded Workbench® for Renesas Synergy ™ development environment and compiler available to developers. Engineers that have been using e2 Studio might be hesitant to convert their e2 projects into IAR Workbench projects. Doesn’t this seem like it ...

    Jan 26, 2017
  2. Coming up to Speed with e2 Studio 5.2.1 New Features

    ... leave the remaining features to the reader to explore.   Figure 1 – New Features and the Benefits A great addition to the recent release is that e2 Studio now supports C++ (IAR Embedded Workbench for Renesas Synergy™ also has added support)! The support is compatible with the recent SSP 1 ...

    Feb 2, 2017
  3. Can any one share me sample project for CAN application for Renesas Synergy™ Starter Kit SK-S7G2 R7FS7G27H3A01CFC

    Hi Team, I am using Renesas Synergy™ Starter Kit SK-S7G2 R7FS7G27H3A01CFC.I am using e2studio and SSP V1.3.3. Can any one share me sample project for CAN application. can you please help me as soon as possible.

    Feb 24, 2018
View All Results from Support Communities (32)

Knowledge Base

  1. Command-line build of e² studio project

    ... command lineThe following manual explains about launch options of eclipsec.exe (or e2studio.exe) and the ini file: Eclipse Platform Help - Runtime optionsIn the projects for Renesas Synergy™ devices, add the following line in the eclipse.ini file (after the line -vmargs) :-Dcom.renesas.synergyLicenseFile= Mar 25, 2024

  2. Differences between e² studio and CS+ Integrated Development Environments

    ... studio, CS+. For more information, see the IDE Release Notes and the respective documentation. [Supported Device Families]e² studioCS+ (CS+ for CC) CS+ (CS+ for CA,CX) RX, RL78, RH850,RA, RZ, RE,Renesas Synergy™,RISC-V MCU RX, RL78, RH850 RL78, 78K, V850 [Supported Compilers]e² studio ...

    Oct 9, 2024
  3. GNU compilers for e² studio

    ... Software Support Package (Synergy SSP) can be selected at installation of e² studio  downloaded from the Renesas Synergy™ Platform site.  Please visit Renesas Synergy™ Platform - Development tools for the details about Synergy SSP. [RZ family]  “GNU ARM Embedded Toolchain” is freely available (see Note 2) for e² studio ...

    Apr 8, 2019
View All Results from Knowledge Base (6)