Skip to main content
Renesas Electronics Corporation

Overview

Description

Renesas recommends three emulator models that support real-time debugging on the actual chip using the debugging functionality built into the Renesas MCU mounted in the user system. Each of them can be used as flash programmers. They range from an affordably priced model which is compared with full-spec emulators and is suitable for education, initial evaluation to more advanced models with functions to support full-scale development work.

Features

  • Lineup [Learn More]
    • E2 emulator
    • E2 emulator Lite
    • E20 emulator

Target Devices

Documentation

Lineup

Image
E2 emulator
Image
E2 emulator Lite
Image
E20 emulator
Image
IDE notes

See other than the above of on-chip debuggers.

Design Support

On-chip Debuggers Information for Users

Information on the discontinuation of E1 emulator production and on its successor products

We have already discontinued production of the E1 emulator due to components of the product having reached their EOL (end of life, i.e. end of production). Please click on the following link to confirm the details and our successor products.

>> Tool News: [Notification] End of Life (EOL) Notice for E1 Emulator (PDF | English, 日本語)

Support

Support Communities

  1. Notification: End of Life Notice for the E20 On-Chip Debugger (R20TS1088)

    For those who take advantage of the RX external trace output capability, keep this notice in mind. [Notification] End of Life (EOL) Notice for the E20 On-Chip Debugger

    Dec 6, 2024
  2. Memory access on R5F72560R

    Hello together!I`m a realy newbi on everykind on renesas mpc`s, so i`m thankfull for every kind of help!Actually i work on a controll device that is equiped with an sh2a 72560r. The problem is, i cant find any manual or an mpc pinout in general ...

    Feb 17, 2021
  3. Getting up to speed on the RL78 with Lora application in mind.

    Hello Forum, Im working on getting up to speed on the E2Studio tool for running an RL78 for low power Lora applications.  I have the E2studio setup in a stand alone config for the RL78.  Im struggling to import the r11an0537ej0102-rl78-lora.zip sample project into the E2studio.  I ...

    Aug 23, 2022
View All Results from Support Communities (370)

Knowledge Base

  1. About RAM-ECC function (on-chip debugger is enabled)

    The RAM -ECC function is enabled when the CPU is activated in normal operation mode (the CPU is not connected to the on-chip debugger) even if the on-chip debugger is enabled.

    Jan 16, 2018
  2. About operation of safety functions when using on-chip debugger

    ... impossible to evaluate this function with the on-chip debugger. ∙ A/D test function: It is possible to evaluate this function with the on-chip debugger. ∙ Digital output signal level detection function for I/O ports: It is possible to evaluate this function with the on-chip debugger.

    Jan 16, 2018
  3. How is on-chip debug option byte set for program in mass-production?

    ... is to be input when the on-chip debugger is started up. Therefore, as long as "Disabling on-chip debugger operation" is set, the on-chip debug security ID setting is irrelevant. *Note 2Since the on-chip debug security ID must be matched to start up the on-chip debugger ...

    Jul 4, 2013
View All Results from Knowledge Base (38)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?