2023年5月11日
このビデオについて
This video demonstrates a rechargeable toy car with push-to-start and hold-to-stop functionality, built using the SLG47105 HVPAK. The design provides constant motor voltage regardless of battery charge and ensures the car automatically turns off if it gets stuck, helping save battery power. The implementation also includes CC/CV battery charger control. For full details and design files, refer to the complete application note.