メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)

Bluetooth Low Energy Smart Data Logging Label Demonstration

NOTE:

  • The logging process is on hold while the label is connected
  • Erase the logged data before disconnecting for correct timestamping and logging
  • Set and verify the system time
  • Do not trigger a new command while a previous one is active

Simple steps to follow:

  1. Press the push-button on the label for >3s and release.
  2. To turn the label off, please connect the label to a device running the web-app by scanning for and connecting to the label first and pressing the off-button.
  3. Scan for labels and pair to read the logged data.
画像
Bluetooth® Low Energy Smart Data Logging Label Demonstration