2026年5月14日
このビデオについて
Capacitive touch design has a well-earned reputation for unpredictability — and CapExt is built to change that. This webinar walks through how CapExt simulates complete PCB layouts for capacitive touch and analog applications using only Gerber design files as input, delivering actionable results in minutes without requiring extensive setup or specialist simulation expertise. Learn how the tool's fast, low-friction workflow can replace months of iterative prototyping, surface potential in-field issues early in the design cycle, and give electrical engineers the confidence to finalize touch layouts before committing to hardware.