概要
The ZMID5201STKIT is an all-in-one starter kit, providing fully-functional evaluation of the ZMID5201 position sensor. While different position sensor kit types can be ordered separately, this kit combines the linear, rotary, and arc types into a single kit, along with the communications board required to interface with the control software.
特長
• ZMID-COMBOARD communications board
• ZMID5201MLIN01201 linear application module
• ZMID5201MROT36001 rotary application module
• ZMID5201MARC13001 arc application module
• Micro B USB Cable
• 2 x interface cables
サンプル&ご購入
Absolute arc with 130-degree range
ZMID5201STKIT 廃止品
| Pb (Lead) Free: | Yes |