概要
The ZMID5201MROT is an inductive rotary position sensor module including sensor PCB, target and target holder.
NOTE: This module is pre-programmed and characterized. For changing programming options, such as motion range or diagnostic settings, the ZMID communication board (ZMID-COMBOARD) is required.
特長
- Contactless
- High-resolution angle position measurement
- Analog voltage output
- Strayfield-immune
サンプル&ご購入
Rotary on-axis with 360-degree range
ZMID5201MROT36001 廃止品
| Description: | Rotary on-axis with 360-degree range |