概要
The Ethernet Extension Board for 1000BASE-T1 (Marvell 88Q2112 Transceiver) can be used with the RH850 Generation 2 Mainboard (Y-RH850-X2X-MB-T1-V1) of the RH850 Evaluation Platform and the Common Mainboard (Y-COMMON-MB-T1-V1) of the common RH850 and R-Car MCU Evaluation Platform.
特長
- Ethernet extension board with Marvell 88Q2112 1000BASE-T1 transceiver
使用製品


サンプル&ご購入
Y-COMMON-1000BASE-T1-88Q2112
アクティブ| Pb (Lead) Free: | No |