メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation) - 6月はプライド月間として、LGBTQ+の権利や文化、コミュニティについて啓発する世界的な活動月間です

概要

説明

The Renesas USB to PMBus adapter (often referred to as a "dongle") is used to connect a demonstration board with a PMBus interface to a PC. The USB to PMBus adapter is powered from the USB output of the host PC. The USB interface utilizes the USB Mini format, and the output uses a standard 2 row, 6 pin header on 0.100 inch centers. The PMBus command set is accessed by using the PowerNavigator™ evaluation software from a PC running Microsoft Windows.

The ISLUSBEVAL1Z is the replacement part for ZLUSBEVAL3Z which is now end of life (EOL).

特長

  • Connect the USB Mini provided between the host computer and the USB to PMBus adapter
  • Connect USB to PMBus adapter to demonstration board to test or evaluate
  • Apply input power (labeled VIN) to the demonstration board
  • Using the host PC's internet browser, navigate to the PowerNavigator™ software page.
  • Follow the download instructions.
  • Once the PowerNavigator™ software is installed, double-click on the PowerNavigator™ icon and follow the software's instructions.

アプリケーション

ドキュメント

設計・開発

ソフトウェア/ツール

ソフトウェアダウンロード

製品選択

Part NumberStatusStockBudgetary Price (USD)SampleablePb (Lead) FreeECCN (US)HTS (US)
ISLUSBEVAL1ZActiveIn Stock1u | $77.8AvailableYesEAR998473.30.1180