メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)

概要

説明

The MicroClock  5X1503/5X1503L/5X1503S Development Kit includes a USB interface connecting board, 5X1503/ 5X1503L/5X1503S evaluation board, tiny evaluation board, and 25 units of 5X1503 samples. Using the Renesas Timing CommanderTM graphical user interface (GUI), customers can create their own sample in minutes and also perform signal integrity verification on the board. Renesas Timing CommanderTM GUI can be used to upload or program the 5X1503 series on the board through a USB interface connecting board.

特長

  • Program MicroClock 5X1503 / 5X1503L / 5X1503S blank parts in the socket
  • Removable socket board
  • Programmer board is powered using USB port
  • Programmer board uses Renesas Timing CommanderTM GUI to program the blank parts
  • USB port is the communication channel between the GUI and the MicroClock 5X1503 series devices in the socket
  • A tiny evaluation board can be attached to an existing system for system validation

アプリケーション

ドキュメント

設計・開発

ソフトウェア/ツール

製品選択

Part NumberStatusStockBudgetary Price (USD)SampleablePb (Lead) FreeECCN (US)HTS (US)
DEV5X1503ActiveIn Stock1u | $79AvailableNoEAR998473.30.1180

ビデオ&トレーニング