May 1, 2026
About This Video
Learn how to configure and use Universal Asynchronous Receiver/Transmitter (UART) communication on the RA8E1 Prototyping Board (FPB‑RA8E1) Arm® Cortex®‑M85 entry‑line MCU. The UART peripheral is configured using the Flexible Software Package (FSP), including communication parameter configuration and the implementation of transmit and receive functionality. Data is exchanged between the board and a host system through a serial terminal, allowing users to observe and verify communication in real time.