Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The Renesas integrated development environment, or the High-performance Embedded Workshop, supports Tcl/Tk Version 8.4.4. Tcl/Tk is comprised of a class member "Tcl" of script language (Tool Command Language) and the "Tk" (Tool Kit) used to program a graphical user interface. Use of Tcl/Tk helps to create appropriate GUIs that suit the development environment, in addition to the functions and GUIs supplied by the High-performance Embedded Workshop, thereby extending the development environment further.

Learn More

Target Devices

Type Title Date
Release Note PDF 307 KB 日本語
Manual - Development Tools PDF 4.16 MB 日本語
Manual - Development Tools PDF 1.85 MB 日本語
Application Note PDF 1.43 MB
AI-generated Summary: Renesas provides guidelines and disclaimers regarding the use of its products and information. It emphasizes that the information is for reference only, without warranties or liability for damages. Use in military, life-support, healthcare, or safety-critical systems is prohibited without prior consultation. Users must adhere to specified operating ranges and implement safety measures to prevent failures and accidents. Renesas disclaims liability for misuse or use beyond specifications and requires safety evaluations for final products.
4 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 17 KB 日本語
Sample Code
Log in to Download ZIP 9 KB 日本語 IDE: HEW
Sample Code
Log in to Download ZIP 14 KB 日本語
3 items

Functions

The High-performance Embedded Workshop offers a Console window that supports Tcl/Tk programming and a GUI window.

Image
Tcl/Tk startup screen

Tcl/Tk startup screen

Usage and a list of commands

The Console window of the High-performance Embedded Workshop permits Tcl/Tk programming to be performed in interpreter mode or script file load mode.

Interpreter mode
Tcl/Tk commands are executed by entering them directly in the Console window.
Script file load mode
A Tcl/Tk script file created beforehand is loaded and executed in the Console window.

During programming with Tcl/Tk, various commands supported in the High-performance Embedded Workshop environment can be used. By using Tcl/Tk and these commands in combination, it is possible to create GUIs that control the High-performance Embedded Workshop environment.

[Example of High-performance Embedded Workshop Usable in Tcl/Tk]

  • Execution relevance
  • Download relevance
  • Register relevance
  • Memory relevance
  • Assemble/Disassemble relevance
  • Break relevance
  • Trace relevance
  • Coverage relevance
  • Performance measurement relevance
  • Script/log file relevance
  • Map relevance
  • Simulation configuration relevance
  • Standard I/O and file I/O relevance
  • Utility relevance
  • Projects and Workspace relevance

The usable commands of the High-performance Embedded Workshop differ with the target MCU for which the simulator and emulator are used. For details on how to use, refer to Tcl/Tk Application Notes.

Basic Sample Programs

Basic Tcl/Tk sample programs are supplied from Renesas. Use these samples to understand the basic method of programming.

Tcl sample program
This sample program uses the basic commands of Tcl. Download (Tcl sample program)
Tk sample program
This sample program uses the basic commands of Tk. Download (Tk sample program)
Image
Tk sample program images

Tk sample program images

Sample control program

A Tcl/Tk sample program to control the High-performance Embedded Workshop is supplied from Renesas. It creates a GUI with Tcl/Tk to control the High-performance Embedded Workshop.

Image
Conceptual image of a sample control program

Conceptual image of a sample control program

Support Communities

  1. Unit testing in Renesas HEW

    I have been searching for ways / tools to unit test in Renesas HEW. After a quick search on the internet, I can see that HEW has a tool (sort of a TCL / Tk plugin) to do this, as described here. Although, after exhaustive search, unfortunately I could not ...

    Jun 18, 2014