Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Renesas Electronics Corporation

Category: Communication

For the Synergy MCU configured as a Communications Device Class (CDC) device to be recognized by the Windows® (7/8/10) host PC, the Synergy signed USB CDC driver must be installed on the Windows host PC.

The Synergy signed USB CDC driver supersedes all previous versions of the Synergy USB CDC drivers. The driver package consists of the catalog (.cat) and installation information (.inf) files along with an application note with instructions for installing the Synergy signed USB CDC drivers on the Windows host PC.

The Synergy signed USB driver is created with the following USB Vendor and Product ID:

  • Vendor ID: 045B
  • Product ID: 5300 (dedicated for Synergy USB CDC class)
  • Class Code: Miscellaneous

Release Information

USB CDC Drivers v 0.1

Current Public Release

Release Date: 2018-04-12

MD5: b405aee4c406534f52014fc6367fe78d

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 619 KB
1 item
Type Title Date
Application Note PDF 616 KB
1 item

Support Communities

  1. Synergy Signed USB CDC Driver

    Zip file of USB CDC Driver material

  2. USB-CDC driver: how to use with Windows XP?

    Have a request to use our system (uses S5D9) over USB-CDC on Windows XP host. Presently works well on Win7-10. Is there a earlier version of the driver that will work with XP? Or are there any work-arounds or virtualization to allow connection to XP system? These ...

    Jun 2, 2021
  3. Renesas VID PID fo USB CDC

    Renesas provides a signed USB CDC driver (for Windows OSs). https://www.renesas.com/kr/en/products/synergy/software/add-ons/usb-cdc-drivers.html This driver is created for VID: 045B (Renesas Electronics Corp) and PID: 5300, and it seems ...

    Apr 12, 2019
View All Results from Support Communities (18)

Knowledge Base

  1. How do I set-up USB drivers for Synergy CDC-ACM projects Windows 7 and Windows 8?

    ... signed driver should show up in the Model list as Synergy USB CDC/ACM. Click Next. Ignore any Warnings and continue to install the driver. The driver should now be installed and will show up in the Ports (COM & LPT) list as seen below.     [Tags]   CDC-ACM,   Synergy ...