Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

RZ/V2N AI Software Development Kit (AI SDK) is an AI application development environment for the RZ/V2N Evaluation Board Kit.

Please see the following webpage for more details.
https://renesas-rz.github.io/rzv_ai_sdk/latest/

Image
RZ/V2N AI Software Development Kit (SDK)

AI SDK provides the following packages.

PackageDetails
AI SDKPackage used for AI Development.
​Users can build/run the AI Application easily and quickly.
AI SDK Source CodePackage used for Linux Development.
Users can customize the Linux environment and develop their own board.

Features

  • AI Software Development Kit (AI SDK) is a solution that allows you to develop AI applications easily and quickly using Renesas' RZ/V evaluation boards (RZ/V2N-EVK).
  • AI SDK includes Yocto Linux with bootloader, Linux kernel, cross compiler and a complete set of libraries for DRP-AI, graphics, video codec and OpenCV Accelerator. USB/MIPI camera can be used with Video for Linux 2 (V4L2) API.
  • By using the AI SDK Source Code, you will be able to change the source code and customize the Linux environment.

Release Information

  • 2026/3/31: RZ/V2N AI SDK v6.30
  • 2025/6/30: RZ/V2N AI SDK v6.00
  • 2025/3/11: RZ/V2N AI SDK v5.00

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 3,670.27 MB
Software & Tools - Software
Log in to Download ZIP 4,071.49 MB
Software & Tools - Software
Log in to Download ZIP 4,041.79 MB
Software & Tools - Software
Log in to Download ZIP 3,475.82 MB
Software & Tools - Software
Log in to Download ZIP 2,593.11 MB
Software & Tools - Software
Log in to Download ZIP 16,033.74 MB
6 items
Type Title Date
Release Note PDF 190 KB
Release Note PDF 133 KB
Release Note PDF 131 KB
3 items

Related Boards & Kits

Renesas provides support for the items listed below for the RZ/V2N AI Software Development Kit at no additional cost.

 FormQ&A and Issue Analysis1Maintained by Renesas
Renesas Reference BoardCustomer Board
Customer Developed/Modified Software

-

No

No2

No

Customer Added OSS

-

No

No

No

Renesas Developed Software

Source Code

Yes

Yes

Yes

Binary

Yes

Yes3

Yes

Notes:
1. First, customers should investigate which component has an issue—whether it is a Renesas deliverable or a customer-developed component.
2. We provide support for board-dependent changes such as channel numbers and pin configurations.
3. We provide Q&A support only for functions that are defined and described in the user's manual.