Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

QE for Motor: Development Assistance Tool for Motor Applications Information for Users

QE for Motor: Development Assistance Tool for Motor Applications

Updating QE for Motor [RA] from V1.0.0 to V1.1.0 or a later version

If you have already installed V1.0.0 of QE for Motor [RA] on your PC and wish to update it to V1.1.0 or a later version, select either of the following methods.

warningThe [Open the Update >>] link (shown below) in the [Motor Main (QE)] view of QE for Motor [RA] V1.0.0 cannot be used in updating that version to V1.1.0 or a later version.
However, after you have updated V1.0.0 to V1.1.0 or a later version, you can use the [Open the Update >>] link for further updates.
Image
qemotor-update-en

 

 

Download the latest version of QE for Motor from the Renesas Web site and install it

Follow the procedure below to download the latest version of QE for Motor from the Renesas Web site and install it.

  1. Download the latest version of QE for Motor from the “QE for Motor” product page.
    QE for Motor >>
  2. Select the downloaded file to install QE for Motor.
    According to the instructions given on the QE: Tools for Particular Applications Information for Users | 1. Download and install QE from the web page, click on the [Archive...] button on the [Add Repository] dialog box and select the .zip file you have downloaded in step 1.

 

Uninstall V1.0.0 of QE for Motor [RA] and use the Renesas Software Installer of the e² studio to install the latest version of QE for Motor

Follow the procedure below to uninstall V1.0.0 of QE for Motor [RA] and use the Renesas Software Installer of the e² studio to install the latest version of QE for Motor.

  1. Uninstall V1.0.0 of QE for Motor [RA].
    Uninstall V1.0.0 of QE for Motor [RA] according to the instructions given on the QE: Tools for Particular Applications Information for Users | Uninstallation page.
  2. Use the Renesas Software Installer of the e² studio to install the latest version of QE for Motor.
    Install the latest version of QE for Motor according to the instructions given on the QE: Tools for Particular Applications Information for Users | 2. Install QE from Renesas Software Installer in e² studio page.