Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Monitor Program for M32C/80, M16C/80 and M16C/60 Series. After the Monitor Program is written to the MCU and the Monitor Program communicates with the Debugger, the user program can be debugged.

Features

  • Use RS-232C for communication between the Debugger and the Monitor Program.
  • When debugging with the Debugger, write the Monitor Program to the MCU using a flash programmer (ex. M16C Flash Starter).
  • Monitor Program for M32C/80, M16C/80 and M16C/60 Series
  • Learn More

Target Devices

Type Title Date
Upgrade - IDE
Log in to Download ZIP 14.57 MB 日本語
Upgrade - IDE
Log in to Download ZIP 66.81 MB 日本語
Upgrade - Debugger
Log in to Download EXE 79.99 MB 日本語
Upgrade - Debugger
Log in to Download EXE 67.49 MB 日本語
Upgrade - Debugger
Log in to Download ZIP 2.88 MB 日本語
Upgrade - Other
Log in to Download ZIP 38 KB 日本語
Upgrade - Other
Log in to Download ZIP 6 KB 日本語
Software & Tools - Other
Log in to Download ZIP 62 KB 日本語
Upgrade - Debugger
Log in to Download ZIP 5.67 MB 日本語
Upgrade - Debugger
Log in to Download ZIP 5.59 MB 日本語
Software & Tools - Other
Log in to Download ZIP 21 KB 日本語
Upgrade - Other
Log in to Download ZIP 20 KB 日本語
12 items

System Configuration

Image
System Configuration

Preparations

  • PC with Serial Port
  • Communication Cable
  • Target Board, Power Supply
  • Flash Programmer (for writing the monitor program to the MCU)
  • Monitor Program
  • Debugger

* You can download the Monitor Programs and the Debuggers from the "Documentation & Downloads".

Operating Environment

The operating environment depends on your debugger.

M16C R8C FoUSB/UART debugger (High-performance Embedded Workshop Version),
M32C FoUSB/UART debugger (High-performance Embedded Workshop Version)

ItemDescription
PCIBM PC/AT or compatible PC with Intel Pentium III 600MHz or higher
OSWindows XP, Windows 2000, Windows ME, Windows 98 SE (98)
Memory128MB or higher
Interface9-pin D-SUB Serial Interface

M16C R8C FoUSB/UART debugger (KD30 Version),
M32C UART debugger (KD308 Version),
M32C FoUSB/UART debugger (KD3083 Version)

ItemDescription
PCIBM PC/AT or compatible PC with Intel DX4 100MHz/Pentium II 75MHz or higher
OSWindows XP, Windows 2000, Windows ME, Windows 98 SE (98), Windows 95
Memory16MB or higher
Interface9-pin D-SUB Serial Interface

Debugging Method

Image
Debugging Method

Debugging Communication Port

The serial port of MCU is used for communication between the monitor program and debugger.
The serial port used by the monitor program is shown below.

MCUChannelRxD (Reception)TxD (Transmission)*
M16C/62A, 62M1P6_6/RxD1P6_7/TxD1* Please connect a pull-up resistor (approx. 5kΩ) to the TxD pin.
M16C/801P6_6/RxD1P6_7/TxD1
M32C/831P6_6/RxD1P6_7/TxD1

The monitor program offered by Renesas uses the same serial port as the flash programmer supporting Renesas Standard Serial I/O Mode 2 (serial programming mode). Therefore, if the circuit for reference use of the flash programmer which supports Standard Serial I/O Mode 2 is used, you can easily create the environment from writing the monitor program to MCU to debugging.
Renesas provides M16C Flash Starter as a flash programmer supporting Standard Serial I/O Mode 2.

Debugging Memory Map

M16C/62A, M16C/62M Group

Example: M30624FGA (ROM:256KB, RAM:20KB)

Image
M16C/62A, M16C/62M Group Debugging Memory Map

M16C/80 Group

Example: M30800FC (ROM:128KB, RAM:10KB)

Image
M16C/80 Group Debugging Memory Map

M32C/83 Group

Example: M30833FJ (ROM:512KB, RAM:31KB)

Image
M16C/83 Group Debugging Memory Map

Upgrade Information

Debugger (High-performance Embedded Workshop version / KD version)

<<KD debugger does not have a plan to revise any more.>>

* Target product : M32C M16C UART Monitor Program | R8C UART Monitor Program

High-performance Embedded Workshop version

[Latest Version]

  • Released Date : 1. July, 2007
  • Software name :
    • M16C R8C FoUSB/UART Debugger
    • M32C FoUSB/UART Debugger
  • Version : V.1.03 Release 00
  • New feature(s)
    • Comes with High-performance Embedded Workshop V.4.03.00
    • [Disconnect] function
    • Representational function of instruction format specifier in disassembly language
    • Assignment function to bit-field members
    • Some more improvements

[How to upgrade to the latest version]
Download free updates from the "Documentation & Downloads". Upgradable from any previous versions.

[How to install]
Each emulator and monitor debugger is not bundled with High-performance Embedded Workshop. Please download from the "Documentation & Downloads" on this page. Installing this emulator debugger add High-performance Embedded Workshop environment a debugging function.

KD version

[Latest Version]

Released DateSoftware nameVersion
9. June, 2004KD30
(M16C R8C FoUSB/UART Debugger)
Ver.4.10 Release 1
25. August, 2004KD3083
(M32C FoUSB/UART Debugger)
Ver.3.30 Release 1
28. May, 1999KD308*
(M32C UART Debugger)
Ver.1.00 Release 1

* KD308 is a M16C/80 Group debugger for "M32C M16C UART Monitor Program". This product has no plan to support High-performance Embedded Workshop in the future.

[How to upgrade to the latest version]
Download free updates from the "Documentation & Downloads".

Target Devices

The debugger depends on your MCU. In addition, the High-performance Embedded Workshop version of the debugger is the successor debugger of the KD30/KD3083 version. The High-performance Embedded Workshop version is only scheduled for release in the future.

M16C R8C FoUSB/UART debugger (High-performance Embedded Workshop Version) or
M16C R8C FoUSB/UART debugger  (KD30 Version)

FamilySeriesGroupPart No.
M16CM16C/60M16C/62AM30624FGAFP/GPM30625FGAGP
M16C/62MM30624FGMFP/GPM30625FGMGP

M32C FoUSB/UART debugger (High-performance Embedded Workshop Version) or
M32C FoUSB/UART debugger(KD3083 Version)

FamilySeriesGroupPart No.
M16CM32C/80M32C/83M3033FJFP/GPM30835FJGP

M32C UART debugger(KD308 Version)

FamilySeriesGroupPart No.
M16CM16C/80M16C/80M30800FCFP/GPM30802FCGP

Support Communities

  1. Debugger for M16C/62A

    Hello everyone,I have some old M30624FGAFP (M16C/62A). I like to play a little with them, but I have a problem. When I open a project in HEW I can select this device easily, but when I like to connect to the device with an E8A, there is ...

    May 5, 2010
  2. R8C/15 R5F21154 how to write via UART.

    ... UART to my MCU? I have looked at a lot of information on the Internet, but I haven’t found what I need. The FDT program has this MCU, but it only works with E8A, and I don't have it, I need to write and read through the UART ...

    Apr 24, 2021