Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The I/O DLL kit provides a means for extending the functions of the simulator debugger in the High-performance Embedded Workshop integrated development environment (IDE). This kit supports the creation of I/O DLLs. The I/O DLL refers to a DLL (Note1) that operates in cooperation with the simulator engine of the simulator debugger.

Once the necessary settings are made, the simulator debugger allows you to load an I/O DLL and operate it synchronously with the timing at which instructions are single-stepped, memory is read or written or an interrupt occurs. That way, the operation of the input/output ports or the internal peripheral functions of the microcomputer can be simulated as a means of debugging the target program. Furthermore, linked operation with an external tool can be realized by, for example, sending and receiving data to and from that tool.

Any desired I/O DLL can be created by using C/C++ language. To create an I/O DLL, you need to have Microsoft Visual C++, a Windows application development environment available on the market.

Note

  1. DLL is the acronym of Dynamic Link Library. This is a function of the operating system that allows you to save executable routines (routines that supply a specific function or a set of functions) to be saved separately as a file with the extension ".dll". These routines are loaded only when they are needed by the calling program.

Learn More

Target Devices

Type Title Date
Software & Tools - Other
Log in to Download EXE 2.32 MB 日本語
Software & Tools - Other
Log in to Download EXE 1.81 MB 日本語
2 items
Type Title Date
Release Note PDF 68 KB 日本語
Manual - Development Tools PDF 359 KB 日本語
2 items

Linkage Between the Simulator Engine and I/O DLL

The simulator engine calls the functions that have been predefined on the I/O DLL side synchronously with the timing shown below:

  • After executing one instruction (number of execution cycles)
  • Before execution (PC value)
  • When the target is reset
  • When an interrupt occurs
  • Immediately before memory read (address information)
  • Immediately after memory write (address information)

Conversely, the following functions that have been made public for the simulator engine can be called from the I/O DLL side:

  • Get memory contents
  • Set a memory value
  • Get a register value
  • Set a register value
  • Interrupt occurrence
  • Confirm interrupt occurrence condition
  • Inspect the total number of cycles executed
Image
Processing flow

Processing flow

Supported Simulator Debuggers

This I/O DLL kit is available for the following simulator debuggers in the compiler packages :

Note: This I/O DLL kit is NOT supported by the M3T-PDxxSIM simulator debuggers. For M3T-PDxxSIM, use the PDxxSIM I/O DLL Kit.

Development Tools Used

To create an I/O DLL, you need to have Microsoft Visual C++, a Windows application development environment available on the market.

Sample Programs

The following sample programs are stored in a location at the hierarchical level below the directory in which this I/O DLL kit is installed. Refer to the release note for details on how to install the I/O DLL kit.

  • I/O DLL to link with Excel from Microsoft Corporation
  • I/O DLL to read/write data from a file
  • I/O DLL to simulate the operation of a microcomputer's internal peripheral functions

Support Communities

  1. M16C Simulator External Stimulus

    ... to read the state of a pin (heating on) and provide the stimulus that the temperature sensor pulled a pin high or low. What is the common way to do that. I/O scripts, the I/O DLL Kit, Hew Target Server ... Thank you for suggestions and examples.

    Jul 27, 2017
  2. Program QSPI Flash DA1469x USB-Kit

    ... nogui -rtos GDBServer/RTOSPlugin_FreeRTOS -----GDB Server start settings----- GDBInit file: none GDB Server Listening port: 2331 SWO raw output listening port: 2332 Terminal I/O port: 2333 Accept remote connection: localhost only Generate logfile: on Verify download: on Init regs on start: on Silent mode: off Single ...

    Jun 17, 2019
  3. Debug fails with "Cannot read register" Error

    ... Unknown command line parameter singlerun found. -----GDB Server start settings----- GDBInit file: none GDB Server Listening port: 2331 SWO raw output listening port: 2332 Terminal I/O port: 2333 Accept remote connection: localhost only Generate logfile: on Verify download: on Init regs on start: on Silent mode: off Single ...

    Mar 8, 2017
View All Results from Support Communities (6)