Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Renesas Electronics Corporation

Category: Development

The Custom Board Support Package Creator is a command-line tool within the e2 studio IDE for creating custom board support packages (BSPs) that ensure proper boot up and application initialization.

This tool is required to migrate an application developed on a Synergy kit to a new board design, a custom BSP enables the MCU to reset to the main application. The custom BSP also provides information to the SSP modules so they can be automatically configured for new hardware.

Features

The Custom BSP Creator application note shows how to use the tool to create an example custom BSP based on the Synergy DK-S7G2 Development Kit in four easy steps:

  • Create base BSP from the existing BSP of the Synergy kit
  • Create a template pack with the base BSP
  • Create a new project in e2 studio to modify the base BSP
  • Create the final pack for the custom BSP

Release Information

Custom Board Support Package (BSP) Creator 1.03

Current Public Release

Release Date: 2016-06-27

MD5: c5529f1759d33bd3c9c7563a54998c35

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 8.43 MB
1 item
Type Title Date
Application Note PDF 439 KB
1 item

Support Communities

  1. Creating a Custom Board Support Package (BSP)

    ... custom code, modules and even framework components! In the next post, we will dive deeper and see how we can add these features to our custom BSP. In the mean-time,   Live long and profit!   Professor_IoT     Hot Tip of the Week   Download the Custom Board Support Package Creator from ...

    Nov 9, 2016
  2. SSP 2.6.1 Custom BSP does not work

    I downloaded and installed the tools from https://www.renesas.com/en/software-tool/custom-board-support-package-creator#overview I am getting Permission errors, so I just tried listing the boards. PS C:\Users\BSP> custom_bsp_creator.exe -p C:/Renesas ...

    Dec 17, 2024
  3. Custom BSP creation

    ... and instructions on custom BSP creation: https://www.renesas.com/en-eu/products/synergy/software/add-ons/custom-board-support-package-bsp-creator.html   However, it's released in 2016 and it seems like I cannot use it. When I try to ...

    Jun 6, 2018
View All Results from Support Communities (12)

Knowledge Base

  1. How do I create a custom Board Support Package (BSP) for an SSP 1.2.0 Project?

    ... board support package (BSP) using a special tool- the BSP Custom Creator Tool. A custom BSP is usually required when you create your own target board. The tool has 4 steps and uses 2 executable functions. 1) Create a base BSP from and existing BSP (Custom BSP Creator) 2) Create ...

    Oct 13, 2016