Skip to main content
Renesas Electronics Corporation

Synchronous FIFOs

Renesas synchronous FIFO products feature clocked read/write controls, along with two fixed flags (empty, full) and two programmable flags (almost-empty, almost-full). Our synchronous FIFO solutions are ideal for applications that require high-volume data buffering, such as networking, video, telecommunications, local area networks (LANs), and data communications. These devices support depth expansion through a daisy-chain configuration.

About Synchronous FIFO

About Synchronous FIFO

Synchronous FIFOs buffer and queue data, ensuring the first byte at the input is the first released at the output. FIFOs are typically implemented as circular queues with both read and write pointers. Unlike asynchronous FIFOs that use asynchronous signals, synchronous FIFOs rely on clocks to synchronize CPUs with other hardware, enabling efficient, sequential data flow in diverse applications.