Skip to main content
Renesas Electronics Corporation

Overview

The ZMID5202MARC is an inductive arc position sensor module including sensor PCB, target and target holder.

NOTE: This module is pre-programmed and characterized. For changing programming options, such as motion range or diagnostic settings, the ZMID communication board (ZMID-COMBOARD) is required.

Features

  • Contactless
  • High-resolution arc position measurement
  • Digital PWM output
  • Strayfield-immune

Products in the Design

Sample & Buy

ZMID520x - Arc Evaluation Board (front)

Absolute arc with 130-degree range

ZMID5202MARC13001 Obsolete
Description:Absolute arc with 130-degree range