Skip to main content
Renesas Electronics Corporation

Overview

The Renesas Starter Kit for SH7137 is intended as a user-friendly introductory and evaluation tool for the SH7137 microcontroller. The board provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using High-performance Embedded Workshop as well as programming the device using E10A emulator.

The Renesas Starter Kit for SH7137 may be connected to the host PC using a simple RS232 serial connection or via the included USB E10A on-chip debugging interface.

The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run only minutes from opening box. It can prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.

Notes

Evaluation versions differ from their full-versions in functionality and performance. And technical support services are NOT available.

Learn More (Evaluation Software Tools)

Products in the Design

Sample & Buy

Renesas Starter Kit for SH7137

SH7137-Starter-Kit

Not Recommended for New Designs

Support

Support Communities

  1. SH7137 standard boot loader ( User BOOT MAT)

    Hi guys  while trying to use a board with a SH7137 on it, i connected it via FDT in Boot mode , and now seems like the Boot area is totally cleared (user boot flash is all FF...) ! what i can do now to fix it ?, is there some standard bootloader ...

    Feb 27, 2021